SLVSFU7B July 2022 – April 2024 TPS929240-Q1
PRODUCTION DATA
The TPS929240-Q1 supports both PWM dimming method and phase shift PWM dimming method. In PWM dimming mode, all 24 current output channels are turned on and off together at the same time at PWM dimming frequency set by PWMFREQ register as the following figure illustrates.
The phase shift PWM dimming mode is enabled by setting PSEN to 1. In phase shift PWM dimming mode, every three current output channels are formed as one group, so a total of eight current output groups are turned on and off at PWM dimming frequency set by PWMFREQ register with a constant delay as the following figure illustrates. The detailed group information is also listed in the below table.
| Phase | Groups | Output Channels | ||
|---|---|---|---|---|
| Phase 0 | Group A | OUTA0 | OUTA1 | OUTA2 |
| Phase 1 | Group B | OUTB0 | OUTB1 | OUTB2 |
| Phase 2 | Group C | OUTC0 | OUTC1 | OUTC2 |
| Phase 3 | Group D | OUTD0 | OUTD1 | OUTD2 |
| Phase 4 | Group E | OUTE0 | OUTE1 | OUTE2 |
| Phase 5 | Group F | OUTF0 | OUTF1 | OUTF2 |
| Phase 6 | Group G | OUTG0 | OUTG1 | OUTG2 |
| Phase 7 | Group H | OUTH0 | OUTH1 | OUTH2 |
The phase delay interval is 1/8 of PWM dimming cycle time between two neighboring groups. The phase delay can be calculated with the below equation.

where