SLVSGY6C March 2023 – March 2026 TPSM83100 , TPSM83101L
PRODUCTION DATA
The TPSM83100, TPSM83101, and TPSM83101L have input overvoltage protection which avoids any damage to the device in case the current flows from the output to the input and the input source cannot sink current (for example, a diode in the supply path).
If forced PWM mode is active, the current can go negative until reaching the sink current limit. After the input voltage threshold, VT+(IVP), is reached on the VIN pin, the protection disables forced PWM mode and only allows current to flow from VIN to VOUT. After the input voltage drops under the input voltage protection threshold, forced PWM mode can be activated again.