SLVSI35D September 2024 – March 2026 TPS7C84-Q1
PRODUCTION DATA
Connect a feedforward capacitor (CFF) between the OUT pin and the FB pin. CFF improves transient, noise, and PSRR performance. If a higher capacitance CFF is used, the start-up time increases. For a detailed description of the CFF tradeoffs, see the Pros and Cons of Using a Feedforward Capacitor with a Low-Dropout Regulator application note.
As shown in Figure 7-3, poor layout practices and using long traces at the FB pin results in the formation of a parasitic capacitor (CFB).
CFB, along with the feedback resistors R1 and R2 potentially results in the formation of an uncompensated pole in the transfer function of the loop gain. A CFB value as small as 6pF potentially causes the parasitic pole frequency, given by Equation 8, to fall within the LDO bandwidth and result in instability.
Adding a feedforward capacitor (CFF) creates a zero in the loop gain transfer function that compensates for the parasitic pole created by CFB. Figure 7-4 shows this compensation. Equation 9 and Equation 10 calculate the pole and zero frequencies.
The CFF value that makes fP equal to fZ depends on the values of CFB and the feedback resistors used in the application. This CFF value also results in a pole-zero cancellation. Alternatively, if the feedforward capacitor is selected so that CFF ≫ CFB, then the pole and zero frequencies from Equation 9 and Equation 10 are related as:
In most applications, particularly where a 3.3V or 5V VOUT is generated, this ratio is not very large. Thus implying that the frequencies are located close to each other and therefore the parasitic pole is compensated. A CFF value of approximately 100pF ≤ CFF ≤ 10nF typically helps prevent instability caused by the parasitic capacitance on the feedback node. This CFF range helps even for large VOUT values, where this ratio is potentially as large as 20.