SLVSIJ3A May 2026 – November 2026 DRV81646-Q1
PRODUCTION DATA
The resistance of the load affects how long the channel operates in the linear region before hitting thermal shutdown. The resistance functions similarly to a linear drop-out regulator (LDO), where a higher voltage drop requires the device to dissipate more power.
For example, take a 24V system with a 1A ILIM setting for a 5Ω load versus an 11Ω load. Without current limiting these draw 4.8A and 2.2A respectively, but with the ILIM feature, these regulate to 1A. Use Equation 3 to calculate the linear region resistance of the FET to achieve this 1A current limit:
Rearrange Equation 4 to solve for RDS(ON), then plug in the system values for loads 5Ω and 11Ω:
Use this resistance to calculate the power dissipated inside the DRV81646-Q1 FET:
As in Equation 8 and Equation 9, even though both loads are limited to 1A, the DRV81646-Q1 has to dissipate more power for a 5Ω load than an 11Ω load. This power dissipation directly correlates with the temperature rise of the FET over time. More power dissipated means the channel hits thermal shutdown faster.