SLVSIJ6 October 2025 TPS61388-Q1
ADVANCE INFORMATION
The TPS61388-Q1 enters Auto PFM Mode by pulling the MODE/SYNC pin to logic low for more than five switching cycles. The TPS61388-Q1 improves the efficiency at light load when operating in Auto PFM mode. When the output current decreases to a certain level, the output voltage of the error amplifier is clamped by the internal circuit. If the output current reduces further, the inductor current through the high-side switch will be clamped but not lowered further. Pulses are skipped to improve the efficiency at light load.