SLVSJQ6A September 2025 – June 2026 TMF0064
PRODUCTION DATA
The TMF0064 has an 8-bit CRC stored in the most significant byte of the 64-bit ROM. The bus host can compute a CRC value from the first 56 bits of the 64-bit ROM and compare the CRC value to the value stored within the TMF0064 to determine if the ROM data the bus host receives is error-free. The equivalent polynomial function of this CRC is:
The bus host entirely determines the comparison of CRC values and decision to continue with an operation. No circuitry on the TMF0064 prevents a command sequence from proceeding if the CRC stored in or calculated by the device does not match the value generated by the bus host. Proper use of the CRC can result in a communication channel with a high level of integrity.
Figure 6-21 8-Bit CRC Generator Circuit
(X8 + X5 + X4 + 1)