SLVSK24 August 2026 LMR61430-Q1
PRODUCTION DATA
The LMR61430-Q1 uses two current limits to limit the total load current delivered to the output. These limits are known as the high-side peak current limit (IHS-LIM) and the low-side valley current limit (ILS-LIM). After IHS-LIM is reached, the high-side MOSFET is turned off and the low side MOSFET is turned ON until the inductor current falls below ILS-LIM. This action can result in a reduction in switching frequency and can be referred to as soft current limit. Because of the inductor current is limited to switch between IHS-LIM and ILS-LIM, the maximum output current is very close to the average between these two values. If the load demands a current that is greater than the maximum output current, the output voltage decreases. If the output voltage decreases such that the voltage on the FB pin drops below VHIC, then the device enters into hiccup mode. See also Section 7.3.7.
The high-side current limit in LMR61430-Q1 varies as the duty cycle varies. This behavior is characteristic of peak current mode control and helps avoid subharmonic oscillation at higher duty cycles. Figure 7-4 shows the typical high-side current limit.
The LMR61430-Q1 also implements a negative current limit (ILS-NEG-LIM) to limit the amount of current the low-side MOSFET can sink. After the negative current limit is reached, the low-side MOSFET turns off.