SLVSKC7 September 2026 TAS5832
PRODUCTION DATA
Placing the bypassing and decoupling capacitors close to supply has long been understood in the industry. This applies to DVDD, AVDD, GVDD and PVDD. However, the capacitors on the PVDD net for the TAS5832 device deserve special attention.
The small bypass capacitors on the PVDD lines of the DUT must be placed as close to the PVDD pins as possible. Not only dose placing these device far away from the pins increase the electromagnetic interference in the system, but doing so can also negatively affect the reliability of the device. Placement of these components too far from the TAS5832 device can cause ringing on the output pins that can cause the voltage on the output pin to exceed the maximum allowable ratings shown in the Section 5.1 table, damaging the device. For that reason, the capacitors on the PVDD net must be no further away from the associated PVDD pins than what is shown in the example layouts in the Section 8.2.2 section.