SLVSKR5B February 2026 – May 2026 TLV2886 , TLV886
PRODMIX
Low-noise circuit design requires careful analysis of all noise sources. In many cases, external noise sources can dominate; consider the effect of source resistance on overall op-amp noise performance. Total noise of the circuit is the root-sum-square combination of all noise components.
The resistive portion of the source impedance produces thermal noise proportional to the square root of the resistance. The source impedance is typically fixed; consequently, select op amp and the feedback resistors that minimize the respective contributions to the total noise.
Figure 7-1 shows the noninverting op-amp circuit configurations with gain. Figure 7-2 shows the inverting op-amp circuit configurations with gain. In circuit configurations with gain, the feedback network resistors also contribute noise. In general, the current noise of the op amp reacts with the feedback resistors to create additional noise components. However, the low current noise of the TLVx886 means that the current noise contribution can be ignored.
The feedback resistor values can generally be chosen to make these noise sources negligible. Low impedance feedback resistors load the output of the amplifier. The equations for total noise are shown for both configurations.
For additional resources on noise calculations, visit TI Precision Labs.
where
where