SLVSMN6 October 2026 TMUX122-SEP
ADVANCE INFORMATION
Transition time is defined as the time taken by the output of the device to rise or fall 10% after the address signal has risen or fallen past the 50% threshold. Figure 6-4 shows the setup used to measure transition time, denoted by the symbol tTRANSITION.