SLVSMN6 October 2026 TMUX122-SEP
ADVANCE INFORMATION
Propagation delay is defined as the time taken by the output of the device to rise or fall 50% after the input signal has risen or fallen past the 50% threshold. Figure 6-7 shows the setup used to measure propagation delay, denoted by the symbol tPD.