SLVU491A November 2011 – October 2021 TPS54294
The output voltage ripple of converter 1 on the TPS54294EVM is shown in Figure 4-9. The output current is the rated full load of 2 A.
Figure 4-9 TPS54294EVM Converter 1 Output Voltage RippleThe output voltage ripple of converter 1 on the TPS54294EVM at the start of the Eco-mode™ operation is shown in Figure 4-10 . The output current is reduced to around 200 mA.
Figure 4-10 TPS54294EVM Converter 1
Eco-mode™ Output Voltage RippleThe output voltage ripple of converter 1 on the TPS54294EVM during Eco-mode™ operation at no load is shown in Figure 4-11.
Figure 4-11 TPS54294EVM Converter 1
Eco-mode™ Output Voltage Ripple at No Load