SLVU876A February   2013  – May 2021 TPS65279V

 

  1.   Trademarks
  2. 1Introduction
  3. 2Background
  4. 3TPS65279V Schematic
  5. 4Board Layout
  6. 5Bench Test Setup Conditions
    1. 5.1 Header Description and Jumper Placement
    2. 5.2 Hardware Requirement
    3. 5.3 Hardware Setup
    4. 5.4 Installing Software
    5. 5.5 Software Operation
  7. 6Power-Up Procedure
  8. 7TPS65279V EVM Bill of Materials
  9. 8Revision History

Hardware Setup

After connecting the power supply to J1, turn on the power supply, and connect JP1 to Vin through a 100-kΩ resistor, connect JP2 to Vin through a 100-kΩ resistor, connect JP7 to GND, connect JP8 to GND, the EVM will regulate the output voltages to the values shown in Table 2-1. Additional input capacitance may be required in order to mitigate the inductive voltage droop that may occur during a load transient event.

The output voltage is changed by sending the digital control signal via a PC running the TPS65279V controller software and USB-TO-GPIO interface box. Change the output voltage with the following steps:

  • Connect one end of the USB-TO-GPIO box to the PC using the USB cable and the other end to JP15 of the TPS65279V using the supplied 10-pin ribbon cable as shown in Figure 5-2. The connectors on the ribbon cable are keyed to prevent incorrect installation.
  • Connect the power supply on J1, and turn on the power supply.
  • Run the software as explained in the next section.
GUID-EB8DB9F4-E560-4347-9474-9FC9553567B4-low.gifFigure 5-2 USB Interface Adapter Quick Connection Diagram