SLVUBJ9A July 2020 – October 2020 TPS54JB20
The efficiency of this EVM peaks at a load current of about 6 A and then decreases as the load current increases toward full load. The following images show the efficiency for the TPS54JB20EVM at an ambient temperature of 25°C. Figure 2-1 shows the efficiency over a range of Vin values Figure 2-2 shows efficiency over a range of Vcc values and how the light load efficiency is improved in DCM.
Figure 2-1 TPS54JB20
Efficiency Plot: Internal and External Bias
Figure 2-2 TPS54JB20
Efficiency Plot: FCCM and Skip