SLVUC36 April 2021 TPS23882B
The LaunchPad (not included) running a custom software program can communicate with the TPS23882B1 devices on the TPS23882B1EVM-008. Figure 2-3 shows the advanced setup using LaunchPad.
Figure 2-3 Advanced Setup Using LaunchPadâ„¢If wanting to run TPS23882B1 in semi-auto mode, remove the jumper installed on J5 of the TPS23882B1 daughterboard before powering on the board.
Do not press the RESET button (S1) on the motherboard while communicating over I2C. Pressing this button will set all ports to off mode and the reference code will not be able to recover.