The following procedure outlines the steps to be
taken for using the TPSM33625EVM and TPSM625FEVM.
Use this section in conjunction with Section 3
to correctly setup the EVM.
- Determine the output voltage that is to be
evaluated, then reference Section 2. This table provides the recommended jumper
configurations.
- After making any required changes, confirm that the output voltage is within a couple percent of the set output voltage.
- Verify the performance of the EVM and compare with applicable curves within this user's guide.
- Consult on e2e if there are concerns in the
evaluation of this device.
Table 2-1 Suggested Frequency and Output Voltage
Settings| VOUT (V) | Suggested Frequency |
|---|
| 1.8 | 300 kHz |
2.5 | 800 kHz |
| 3.3 | 1 MHz |
| 5 | 1 MHz (J4: 3 – 4) *2.2 MHz can improve transient response for given output capacitance. |
| 12 | 2.2 MHz |