SLVUCH7A september 2022 – june 2023 TPS25990
The Register Map page as shown in Figure 6-25 enables users to access all the registers supported by TPS25990 eFuse at a glance. Additionally, read and write operations can also be performed here on each register as applicable.
To write into a register if applicable, type the revised value in the field and press ENTER. To read a particular register, select the register and click on the READ REGISTER icon. Click on the READ ALL REGISTERS icon to read all the registers supported by the device at a time.