SLVUCR8B September 2023 – August 2026 TPS25751
| Description | The 'SWSr' Task instructs PD Controller to attempt to become a Source through PR_Swap at the first opportunity while maintaining policy engine compliance. |
|---|---|
| INPUT DATAX | None |
| OUTPUT DATAX | Byte 1: Standard Task Return Code |
| Task Completion | The 'SWSr' Task completes either when the PR_Swap is finished or it is otherwise determined to not be possible or fails. The Task can continue to run because of Wait messages being sent by the Sink. The 'SWSr' Task shall be considered rejected if:
|
| Side Effects | After the SWSr task completes successfully, the PD controller transitions to the Source power role, affecting related registers. If the PR Swap fails after the Accept, the PD specification mandates a subsequent soft and/or hard reset. |
| Additional Information | None |