SLVUCS8 April 2024
The TPS3842 family of devices contain an adjustable reset time delay pin that control the time with which the reset pins de-assert after the pins reach the valid condition. The user can adjust the configuration of these pins via the jumpers located at J2. Position USER of the header connects the pin to a unstuffed 0603 capacitor pad for the user to solder on a capacitor of choice. The capacitor values for these jumpers are labeled on the board and are also listed in Section 2.1.2 and have values of 100pF, 1nF, 0.1uF, 1uF and one with only a pad for user use. Please see the adjustable Reset Time Delay Configuration on the TPS3842 data sheet for more detailed information on user programming.