SLVUDS2 June 2026
The following jumpers are provided to configure the USB-to-I2C adapter:
If operation with an external I2C adapter or microcontroller is desired, the jumpers on J19 can be removed and connections made between the external I2C adapter and the pins on the left-hand side of this header as detailed in Table 2-2. Additional connection points are provided to supply an external pullup supply (V_PU) and to provide an external EN signal to the device. Pin 1 of J19 is the topmost pin on the left side of J19 and is marked with a black dot on the top silkscreen.
Even-numbered pins on the right-hand side of J19 connect to the MSP430F5528. If using an external I2C adapter, TI does not recommend making connections to the even-numbered pins.
| J19 Pin | Electrical Function |
|---|---|
| 1 | V_PU pullup supply |
| 3 | GND |
| 5 | SCL |
| 7 | SDA |
| 9 | RDY |
| 11 | NERR |
| 13 | EN |
| 15 | GND |