SLYA080 july 2023 TMAG5273
In the off-axis method, the magnet is not placed directly above the sensor, which can be any other position within reasonable proximity of the magnet. The placement is shown in Figure 3-5.
Figure 3-5 Off-Axis PlacementThe output and angle changes of the X and Y axes are shown in Figure 3-6:
Considering the installation of knobs and magnets in use, out-of-plane measurement method is common; take the cook-top knob as an example, as shown in Figure 3-7. The Hall sensor is under the knob, and the magnet is inside the knob.
Figure 3-7 Magnet Angle and Hall
Sensor