SLYS029C July 2021 – December 2024 TMAG5110-Q1 , TMAG5111-Q1
PRODUCTION DATA
The device is specified from –40°C to 125°C for a voltage rating of 2.5 V to 38 V. Because the part is draining at its maximum a current of 17 mA the maximum voltage that can be applied will depend on what is the maximum ambient temperature acceptable for the application. The curve in Figure 7-24 shows the maximum acceptable power supply voltage versus the maximum acceptable ambient temperature.
The Figure 7-24 can also be calculated using the following formulas:

where

where

where
Combining the three equations above gives Equation 4 below:

This equation gives the maximum voltage the part can handle in regards of the ambient temperature.
For example, with an the application required to work within a ambient temperature of maximum 85°C, and TJmax, RθJA and ICCmax are defined in the data sheet, the maximum voltage allowed for this application is determined in Equation :

Figure 7-24 Power Derating Curve