SLYT822 March   2022 ISO7710 , ISOUSB211 , TPS25910 , TUSB320LAI

 

  1. 1Introduction
  2. 2Traditional host and peripheral implementations
  3. 3USB Type-C DRP
  4. 4Implementing an isolated USB Type-C DRP
  5. 5Implementation with actual components
  6. 6Demonstration of DRP operation with the ISOUSB211 EVM
  7. 7Conclusion

Demonstration of DRP operation with the ISOUSB211 EVM

This section discusses the implementation of an isolated USB Type-C DRP by combining the ISOUSB211 evaluation module (EVM) and TUSB320-LA-EVM.

In Figure 6-1, the ISOUSB211 and TUSB320LAI together form a DRP. A standard peripheral-like mouse or USB flash drive interfaced with the TUSB320-LA-EVM configured as an upstream-facing port emulates a USB Type-C peripheral. The role of this second TUSB320-LA-EVM is only USB Type-A to USB Type-C conversion. When connected in this fashion, side 1 of the ISOUSB211 EVM is powered by the VBUS output of the PC’s USB port. Side 2 is powered by the isolated DC/DC converter present on the ISOUSB211 EVM. The TUSB320LAI configured as a DRP detects the connection of a peripheral and provides a VBUS supply on the USB Type-C cable. The external peripheral (standard flash drive plus the TUSB320-LA-EVM) detects VBUS on the USB Type-C cable, and proceeds to connect.

The peripheral was able to enumerate, and data communication and transfer was successful.

The TUSB320-LA-EVM uses Schottky diodes in the supply path, which drop about 0.7 V. For proper operation in high-speed mode (when using a flash drive), we connected an external power supply (5.5 V) to the DC_IN terminal of the TUSB320-LA-EVM to account for the 1.4-V voltage drop in the VBUS path across two Schottky diodes. This 5.5-V supply was not needed when using a mouse (low-speed operation).

In Figure 6-2, the ISOUSB211 and TUSB320LAI together form a DRP. A standard host (any laptop or PC) interfaced with the TUSB320-LA-EVM configured as a downstream-facing port emulates a USB Type-C host. The role of this second TUSB320-LA-EVM is only USB Type-A to USB Type-C conversion. Side 1 of the ISOUSB211 EVM is powered by an external 5-V power supply, and the isolated DC/DC converter on the ISOUSB211 is disabled. The TUSB320LAI configured as a DRP detects the connection of a host and does not drive the USB Type-C VBUS. The external host (a standard laptop plus the TUSB320 EVM) detects Rd pulldowns on CC pins and drives the VBUS supply. After VBUS is present on the USB Type-C connector, the peripheral connects.

The peripheral was able to enumerate and data transfer was successful.

An additional 5.5-V power supply was necessary for high-speed operation given the voltage drop across Schottky diodes on the TUSB320-LA-EVM, as explained earlier.

Figure 6-1 The ISOUSB211 and TUSB320 as a DRP connected to a USB Type-C device or peripheral
Figure 6-2 The ISOUSB211 and TUSB320 as a DRP connected to a USB Type-C host