SLYT857 August 2024 TPS1200-Q1 , TPS1211-Q1
Consider this system design example for a 50A load:
The design involves selecting the ISCP and TAUTO-RETRY parameters. For a 50A load design, the ISCP threshold is usually set at 20% above the maximum load current, so in this example, that would be 50A × 1.2 = 60A.
Now, to compute TAUTO-RETRY, see Figure 6 and use the current-voltage relationship of the capacitor at the midpoint of Tcharge/2 to get Equation 6:
where:
and
The time intervals TON1, TOFF1 and TON_mid can be calculated using Equation 9 to Equation 11:
Substituting the known parameters VBATT, Lcable, ISCP, VD1 and CLOAD and solving for TAUTO-RETRY gives a retry delay of <200µs to achieve a charging time of 10ms.
Figure 8 and Figure 9 show the application schematic and test setup to charge a 5mF load capacitance using the TPS1211-Q1 high-side driver. TAUTO-RETRY is 180µs, which results in a charging time of 7ms, as shown in Figure 10.
Figure 9 Test setup using the
TPS1211-Q1 evaluation module with a 1.5m cable harness.
Figure 10 Startup with a 5mF load
capacitance using the TPS1211-Q1 in switching mode.