SLYT876 April   2026 LMH13000

 

  1.   1
  2. 1 Introduction
  3. 2 What makes laser pulse control challenging?
  4. 3 Effects of rise and fall times
  5. 4 Propagation delay
  6. 5 Pulse-to-pulse stability
  7. 6 Implementing precise laser pulse control
  8. 7 Precise pulse control in pulsed systems
  9. 8 Practical example with transmitter test results
  10. 9 Conclusion
  11. 10Additional resources
  12. 11About the authors

Implementing precise laser pulse control

Generating accurate laser pulses requires more than delivering current into the diode. The driver must deliver high peak currents with fast edges, predictable delay and repeatable pulse amplitude. TI's LMH13000 high-speed laser driver generates pulses by converting the input voltage at the VSET pin into a precisely regulated sink current at IOUT, as described by Equation 3. A digital-to-analog converter (DAC) or reference source sets VSET, while the device's internal current mirror and control circuitry regulate the current through the laser diode, as shown in Figure 3. Careful selection of VSET, RSET and the laser anode bias voltage (VLD) allows designers to tune the pulse amplitude, timing and overall pulse stability.

 Circuit schematics transmit path block diagram with a diode and the LMH13000 Figure 3 Circuit schematics transmit path block diagram with a diode and the LMH13000

Here are the design steps for setting pulse current and speed.

  1. Define the target output current (IOUT). Begin with the optical power that the laser diode requires. Equation 3 expresses the peak output current, set by the laser's slope efficiency:
    Equation 3. I O U T = P O P T η

    where POPT is the desired optical output power and η is the laser's slope efficiency (watts per ampere). For example, if POPT = 1W and η = 0.5W/A, then IOUT = 2A.

    Because the LMH13000 supports pulsed currents up to 5A, the selected laser diode must achieve the target optical power at or below this limit. Accurately setting IOUT is paramount for minimizing tpp and reducing amplitude-driven timing errors.

  2. Select RSET and VSET. The LMH13000 sets the output current using the ratio of VSET to RSET, scaled by an internal gain factor k (Equation 4):
    Equation 4. I O U T = V S E T R S E T × k

    In high-current mode (MODE = 1), k ≈ 50k. For example, with RSET = 20kΩ and VSET = 0.8V:

    I O U T = 0.8 20 k × 50 k ≈ 2.0 A

    It is possible to make fine adjustments by trimming VSET with a DAC. Because the LMH13000 regulates current on-chip, this approach minimizes sensitivity to temperature and supply variations, helping keep tpp small within the timing budget.

  3. Set the VLD. VLD must be high enough to support the laser forward voltage and dynamic voltage required during fast current transitions. The LMH13000 data sheet provides Equation 5 as a sizing guideline:
    Equation 5. V L D = V O U T M I N + V F L × d I d t + I O U T × R L A S E R + R D A M P

    where:

    • VIOUT is the minimum compliance voltage at IOUT
    • VF is the forward voltage of the laser at IOUT
    • L is the total loop inductance (package and PCB)
    • dI/dt is the current slew rate (amperes per second) from rise and fall requirements
    • RLASER is the dynamic resistance of the laser diode
    • RDAMP is the external resistance of the laser diode

    For example, with:

    VIOUT(MIN) = 6V
    VF = 2V
    L = 3nH
    d I d t = 2 A 1 n s = 2 × 109 A / s
    RLASER = 0.3Ω
    RDAMP = 1Ω
    V L D ≈ 6 + 2 + 3 × 10 - 9 2 × 10 9 + 2 0.3 + 1.0 ≈ 16.6 V

    A starting value of 17V is therefore appropriate. Increasing VLD improves the edge speed but can increase overshoot, thus requiring careful tuning. Proper VLD selection ensures fast transitions while limiting overshoot, directly reducing the rise and fall time (tr/f) contribution to the overall total timing variation (ttotal) budget.

  4. Optimize rise and fall times and damping. Both driver capability and circuit parasitics set the rise and fall times. Without proper damping, fast current pulse transitions can excite ringing in the laser and PCB loop, causing overshoot and unstable optical pulses. Designers commonly address this by adding a damping resistor and snubber network at the IOUT node. Together, the resistor and snubber suppress parasitic ringing, preserve fast edges, and prevent tr/f from unnecessarily increasing ttotal.

    Select snubber capacitors based on the output capacitance of the driver, calculated using Equation 6:

    Equation 6. C S N U B ≈ 5 × C I O U T

    where CIOUT is the effective capacitance at the IOUT pin. If CIOUT = 40pF, then CSNUB ≈ 200pf.

    Adding a small damping resistor in series with the laser and snubber network suppresses unwanted oscillations. As shown in Figure 4, typical values for RDAMP and RSNUB are in the 5Ω to 10Ω range, with the snubber capacitor sized to the output node capacitance. Select CSNUB for the worst-case (highest) CIOUT, trimming during validation to balance overshoot and edge speed. As illustrated in Figure 5, this approach reduces ringing from fast transitions and PCB parasitics, while preserving the sub-nanosecond tr/f required for precise pulse control.

     Damping resistor and snubber
              network circuit Figure 4 Damping resistor and snubber network circuit

     The LMH13000 pulse with and
              without a snubber circuit or RDAMP

    Figure 5 The LMH13000 pulse with and without a snubber circuit or RDAMP
  5. Control the propagation delay. Unlike rise and fall times, propagation delay is not defined by a formula but instead depends on these layout and interface practices:
  • Input routing. Use differential routing for EP pin and EN pin with 100Ω termination, or route a single-ended input with controlled impedance and proper termination at the LMH13000 input.
  • Output loop. Keep the high-current IOUT loop short and tightly coupled to PGND to minimize inductive delay and ringing.
  • System calibration. Account for any residual system delay by including the driver-laser path in the ToF measurement budget.

As shown in Figure 6, minimizing the trace inductance and ensuring consistent input termination reduces variation in tpd, keeping this contribution small and predictable. For applications that require even higher accuracy or where temperature-based calibration is not practical, Section 6.3.2 of the LMH13000 datasheet presents a technique for high-accuracy start-pulse generation by directly monitoring the laser stage.

 Layout example of the LMH13000 in the surface-mount device package Figure 6 Layout example of the LMH13000 in the surface-mount device package