SNAS872 December 2024 LMR60410
PRODMIX
| PIN | TYPE(1) | DESCRIPTION | |
|---|---|---|---|
| NO. | NAME | ||
| 1 | VIN | P | Regulator input power pin to the high-side power MOSFET and internal VCC regulator. Connect to the input supply and the input filter capacitor CIN. The path from the VIN pin to the input capacitor must be as short as possible. |
| 2 | PGND | G | Power ground. This pin connects to the source of the low-side MOSFET internally. Connect to system ground, and the ground terminal of the CIN and COUT capacitors. The path to CIN must be as short as possible. |
| 3 | SW | P | Regulator switch node. Connect to the power inductor and bootstrap capacitor. |
| 4 | BOOT | P | High-side MOSFET driver supply for bootstrap gate drive. Connect a high quality 100nF capacitor between this pin and SW. |
| 5 | PG | O | Open drain power-good output. Connect to a voltage supply that is an excellent choice through a current limiting pullup resistor. High = regulator OK, low = regulator fault. Goes low when EN = low. See Detailed Description. |
| 6 | FB | I | Feedback pin. Connect this pin directly to the output voltage node for fixed VOUT operation. See Section 4 for the voltage level for each device variant. Connect to the tap point of a feedback voltage divider placed between VOUT node and PGND to program an adjustable output voltage. |
| 7 | MODE/SYNC | I | Operational mode input pin. Tie this pin to the RT pin or suitable supply voltage to select FPWM switching or tie this pin to ground to select PFM switching in light loads. To synchronize to an external clock, connect a 100kΩ resistor to ground and drive directly from the clock. See the Electrical Characteristics table for acceptable voltage levels and timing requirements. |
| 8 | RT | I | Frequency programming pin. A resistor from RT to PGND sets the oscillator frequency between 200kHz and 2.2MHz. |
| 9 | EN | I | Enable pin for the regulator. Drive this pin HIGH to enable the device and LOW to disable the device. If the enable function is not needed, tie this pin to the VIN pin. See the Electrical Characteristics for more information on acceptable voltage levels. |