SNAS876B June 2025 – January 2026 LMR60420-Q1
PRODUCTION DATA
The LMR60420-Q1 uses two current limits to limit the total load current delivered to the output. These limits are known as the high side peak current limit (IHS-LIM) and the low side valley current limit (ILS-LIM). After IHS-LIM is reached on the inductor current, the high side MOSFET is turned off and the low side MOSFET is turned ON until the inductor current falls below ILS-LIM. This action can result in a reduction in switching frequency and can be referred to as soft current limit. Because the inductor current is limited to switch between IHS-LIM and ILS-LIM, the maximum output current is very close to the average between these two values. If the load demands a current that is greater than the maximum output current, the output voltage decreases. If the output voltage decreases such that the voltage on the FB pin drops below VHIC, then the device enters into hiccup mode. See also Section 7.3.7.
The high side current limit in LMR60420-Q1 varies as the duty cycle varies. This behaviour is characteristic of peak current mode control and helps avoid subharmonic oscillation at higher duty cycles. The typical high side current limit is shown in Figure 7-5.
The LMR60420-Q1 also implements a negative current limit (ILS-NEG-LIM) to limit the amount of current the low-side MOSFET can sink. After the negative current limit is reached, the low-side MOSFET turns off.