SNAU182A March 2021 – May 2022
Pin 2 of J12 is connected to the CE pin. Put a short to the HW position, this will connect the CE pin to 3V3 through resistor R38. If the short is placed in the SW position, the status of CE pin is configurable through TICS Pro.
Figure 2-5 J12 Header