SNAU308C November   2024  – August 2026

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  8. 2Hardware
    1. 2.1 Setup
      1. 2.1.1 Evaluation Setup Requirement
      2. 2.1.2 Connection Diagram
    2. 2.2 Jumper Information
    3. 2.3 Power Requirements
    4. 2.4 Reference Clock
    5. 2.5 Output Connections
    6. 2.6 Test Points
  9. 3Software
    1. 3.1 Software Description
    2. 3.2 Software Installation
    3. 3.3 USB2ANY Interface
  10. 4Implementation Results
    1. 4.1 Evaluation Setup
    2. 4.2 Performance Data and Results
      1. 4.2.1 RF Output
      2. 4.2.2 VCO Calibration
        1. 4.2.2.1 No Assist Operation
        2. 4.2.2.2 Full Assist Operation
      3. 4.2.3 SYSREF
        1. 4.2.3.1 SYSREF Clock Generation
        2. 4.2.3.2 SYSREF Pulse Generation
        3. 4.2.3.3 SYSREF Repeater Mode
      4. 4.2.4 Phase Synchronization
        1. 4.2.4.1 Category 1b and Category 2 SYNC
        2. 4.2.4.2 Category 3 SYNC
      5. 4.2.5 Pin Mode
  11. 5Hardware Design Files
    1. 5.1 Schematics
    2. 5.2 PCB Layouts
    3. 5.3 Bill of Materials (BOM)
  12. 6Additional Information
    1. 6.1 Debug Information
    2. 6.2 Trademarks
  13. 7Revision History

USB2ANY Interface

The on-board USB2ANY interface provides a bridge between TICS Pro software and the LMX device. When the on-board USB2ANY controller is first connected to a PC, or if the firmware revision for the controller does not match with the version used by TICS Pro, a firmware update to the controller is required.

  1. Connect the USB cable from the PC to the EVM. The USB interface provides the necessary power to enable the on-board USB2ANY controller.
  2. After Windows has set up a USB device, run TICS Pro in the PC.
  3. The next screen looks like the image below.
    LMX2624SPEVM and LMX2695SEPEVM Firmware Update
                            Request Figure 3-1 Firmware Update Request
  4. Select OK, then the screen looks like the image below. Select Update Firmware.
    LMX2624SPEVM and LMX2695SEPEVM Firmware
                            Loader Figure 3-2 Firmware Loader
  5. Then the screen below appears.
    LMX2624SPEVM and LMX2695SEPEVM Firmware Update
                            Complete Figure 3-3 Firmware Update Complete
  6. Select the Close button to close the window.
  7. A TICS Pro default device pops up. Check to make sure that we get a green light on Connection Mode at the bottom of the GUI.
    LMX2624SPEVM and LMX2695SEPEVM Connection
                            Mode Figure 3-4 Connection Mode
  8. Go to the menu bar, select USB Communications, then select Interface.
    LMX2624SPEVM and LMX2695SEPEVM USB
                            Communications Figure 3-5 USB Communications
  9. Select the Identify button, the LED in the USB2ANY interface flashes.
    LMX2624SPEVM and LMX2695SEPEVM Identify USB2ANY
                            Controller Figure 3-6 Identify USB2ANY Controller
  10. Now, the USB2ANY is ready to use. Select the Close button to close the window.