SNLA419 October 2022 TDP1204 , TMDS1204
This procedure uses the test setup as shown in Figure 2-1. Note, the HDMI 2.1 cables should not be connected immediately, but should be connected as described in Section 3. For more information, see the TMDS1204 EVM User’s Guide as this provides a schematic and an understanding of the functionality of the board before continuing to Section 3. Additionally, the proper software needs to be downloaded onto a personal laptop that includes Total Phase Control Center v4.3.0 and Total Phase USB Driver for I2C/SPI Adapter.