SNLA435A September 2023 – January 2024 DS320PR1601 , DS320PR410 , DS320PR810
To programmatically capture the Eye Scan of varying equalization settings of the PCIe redriver, the following measures must be taken to verify that the capture is valid.
After powering on the PCIe redriver, the following steps can be taken to complete an Eye Scan sweep on a single channel. Please refer to device specific programming guides avaialble on ti.com for further device programming information.
To visualize the captured Eye Scan for the redriver channel, plot each of the 64 DAC hit count values vs. DAC voltage level (or DAC step). This plot is a 90° counter-clockwise rotation of the vertical eye captured at the redriver’s transmitter. An example Eye Scan capture plot can be seen in Figure 3-4, where one EQ boost setting is selected for an Eye Scan capture, then each hit count data point is plotted.

In Figure 3-4, a flat region is observed between the peaks of the hit count plot. This region represents an open portion of the vertical eye observed at the redriver’s transmitter. This can be correlated with an oscilloscope’s eye diagram capture of the same waveform directly after the redriver using the histogram feature of the oscilloscope to plot hits counted at each point along the vertical axis, shown in Figure 3-5. This comparison shows the strong correlation between the oscilloscope’s capture and Eye Scan’s capture of the vertical eye at the redriver transmitter. Please note that the oscilloscope histogram is not to scale.