SNLS458B November 2014 – August 2019 DS90UH929-Q1
PRODUCTION DATA.
| ADD
(dec) |
ADD
(hex) |
REGISTER NAME | BIT(S) | REGISTER
TYPE |
DEFAULT
(hex) |
FUNCTION | DESCRIPTION |
|---|---|---|---|---|---|---|---|
| 0 | 0x00 | I2C Device ID | 7:1 | RW | Strap | DEVICE_ID | 7-bit address of Serializer. Defaults to address configured by the IDx strap pin. |
| 0 | RW | 0x00 | ID Setting | I2C ID setting.
0: Device I2C address is from IDx strap pin (default). 1: Device I2C address is from 0x00[7:1]. |
|||
| 1 | 0x01 | Reset
A software I2C reset command issued by writing to register 0x01 is supported only when operating I2C in the 3.3V mode. |
7:5 | 0x00 | Reserved. | ||
| 4 | RW | HDMI Reset | HDMI Digital Reset.
Resets the HDMI digital block. This bit is self-clearing. 0: Normal operation. 1: Reset. |
||||
| 3:2 | Reserved. | ||||||
| 1 | RW | Digital RESET1 | Reset the entire digital block including registers. This bit is self-clearing.
0: Normal operation (default). 1: Reset. Following the setting of this bit, the software should also set bit 0x4F[1] (BRIDGE_CTL register). This will restore register values that are initially loaded from Non-Volatile Memory to their default state. |
||||
| 0 | RW | Digital RESET0 | Reset the entire digital block except registers. This bit is self-clearing.
0: Normal operation (default). 1: Reset. Registers which are loaded by pin strap will be restored to their original strap value when this bit is set. These registers show 'Strap' as their default value in this table. Registers 0x00, 0x13, 0x15, 0x18, 0x19, 0x1A, 0x48-0x55, 0x58, 0x5B, 0xC0, 0xC2, 0xC3, 0xC6, 0xC8, 0xCE and 0xD0 are also restored to their default value when this bit is set. |
||||
| 3 | 0x03 | General Configuration | 7 | RW | 0xD2 | Back channel CRC Checker Enable | Enable/disable back channel CRC Checker.
0: Disable. 1: Enable (default). |
| 6 | Reserved. | ||||||
| 5 | RW | I2C Remote Write Auto Acknowledge
|
Automatically acknowledge I2C remote writes. When enabled, I2C writes to the Deserializer (or any remote I2C Slave, if I2C PASS ALL is enabled) are immediately acknowledged without waiting for the Deserializer to acknowledge the write. This allows higher throughput on the I2C bus. Note: this mode will prevent any NACK from a remote device from reaching the I2C master.
0: Disable (default). 1: Enable. |
||||
| 4 | RW | Filter Enable | HS, VS, DE two-clock filter. When enabled, pulses less than two full TMDS clock cycles on the DE, HS, and VS inputs will be rejected.
0: Filtering disable. 1: Filtering enable (default). |
||||
| 3 | RW | I2C Pass-through
|
I2C pass-through mode. Read/Write transactions matching any entry in the Slave Alias registers will be passed through to the remote Deserializer.
0: Pass-through disabled (default). 1: Pass-through enabled. |
||||
| 2 | Reserved. | ||||||
| 1 | RW | TMDS Clock Auto | Switch over to internal oscillator in the absence of TMDS Clock.
0: Disable auto-switch. 1: Enable auto-switch (default). |
||||
| 0 | Reserved. | ||||||
| 4 | 0x04 | Mode Select | 7 | RW | 0x80 | Failsafe State | Input failsafe state.
0: Failsafe to High. 1: Failsafe to Low (default). |
| 6 | Reserved. | ||||||
| 5 | RW | CRC Error Reset | Clear back channel CRC Error counters. This bit is NOT self-clearing.
0: Normal operation (default). 1: Clear counters. |
||||
| 4 | RW | Video gate | Set to 1. This prevents video from being sent during the blanking interval. | ||||
| 3:0 | Reserved. | ||||||
| 5 | 0x05 | I2C Control | 7:5 | 0x00 | Reserved. | ||
| 4:3 | RW | SDA Output Delay | Configures output delay on the SDA output. Setting this value will increase output delay in units of 40ns.
Nominal output delay values for SCL to SDA are: 00: 240ns (default). 01: 280ns. 10: 320ns. 11: 360ns. |
||||
| 2 | RW | Local Write Disable | Disable remote writes to local registers. Setting this bit to 1 will prevent remote writes to local device registers from across the control channel. This prevents writes to the Serializer registers from an I2C master attached to the Deserializer. Setting this bit does not affect remote access to I2C slaves at the Serializer.
0: Enable (default). 1: Disable. |
||||
| 1 | RW | I2C Bus Timer Speedup | Speed up I2C bus Watchdog Timer.
0: Watchdog Timer expires after approximately 1s (default). 1: Watchdog Timer expires after approximately 50µs. |
||||
| 0 | RW | I2C Bus Timer Disable | Disable I2C bus Watchdog Timer. The I2C Watchdog Timer may be used to detect when the I2C bus is free or hung up following an invalid termination of a transaction. If SDA is high and no signaling occurs for approximately 1s, the I2C bus will be assumed to be free. If SDA is low and no signaling occurs, the device will attempt to clear the bus by driving 9 clocks on SCL.
0: Enable (default). 1: Disable. |
||||
| 6 | 0x06 | DES ID | 7:1 | RW | 0x00 | DES Device ID
|
7-bit I2C address of the remote Deserializer. A value of 0 in this field disables I2C access to the remote Deserializer. This field is automatically configured by the Bidirectional Control Channel once RX Lock has been detected. Software may overwrite this value, but should also assert the FREEZE DEVICE ID bit to prevent overwriting by the Bidirectional Control Channel.
|
| 0 | RW | Freeze Device ID
|
Freeze Deserializer Device ID.
1: Prevents auto-loading of the Deserializer Device ID by the Bidirectional Control Channel. The ID will be frozen at the value written. 0: Allows auto-loading of the Deserializer Device ID from the Bidirectional Control Channel. |
||||
| 7 | 0x07 | Slave ID[0] | 7:1 | RW | 0x00 | Slave ID 0
|
7-bit I2C address of the remote Slave 0 attached to the remote Deserializer. If an I2C transaction is addressed to Slave Alias ID 0, the transaction will be remapped to this address before passing the transaction across the Bidirectional Control Channel to the Deserializer. A value of 0 in this field disables access to the remote Slave 0.
|
| 0 | Reserved. | ||||||
| 8 | 0x08 | Slave Alias[0] | 7:1 | RW | 0x00 | Slave Alias ID 0
|
7-bit Slave Alias ID of the remote Slave 0 attached to the remote Deserializer. The transaction will be remapped to the address specified in the Slave ID 0 register. A value of 0 in this field disables access to the remote Slave 0.
|
| 0 | Reserved. | ||||||
| 10 | 0x0A | CRC Errors | 7:0 | R | 0x00 | CRC Error LSB
|
Number of back channel CRC errors – 8 least significant bits. Cleared by 0x04[5].
|
| 11 | 0x0B | 7:0 | R | 0x00 | CRC Error MSB
|
Number of back channel CRC errors – 8 most significant bits. Cleared by 0x04[5].
|
|
| 12 | 0x0C | General Status | 7:5 | Reserved. | |||
| 4 | 0x00 | Link Lost
|
Link lost flag for selected port:
This bit indicates that loss of link has been detected. This register bit will stay high until cleared using the CRC Error Reset in register 0x04. |
||||
| 3 | R | BIST CRC Error
|
Back channel CRC error(s) during BIST communication with Deserializer. This bit is cleared upon loss of link, restart of BIST, or assertion of CRC Error Reset bit in 0x04[5].
0: No CRC errors detected during BIST. 1: CRC error(s) detected during BIST. |
||||
| 2 | R | TMDS Clock Detect | Pixel clock status:
0: Valid clock not detected at HDMI input. 1: Valid clock detected at HDMI input. |
||||
| 1 | R | DES Error
|
CRC error(s) during normal communication with Deserializer. This bit is cleared upon loss of link or assertion of 0x04[5].
0: No CRC errors detected. 1: CRC error(s) detected. |
||||
| 0 | R | Link Detect
|
Link detect status:
0: Cable link not detected. 1: Cable link detected. |
||||
| 13 | 0x0D | GPIO0 Configuration | 7:4 | R | Revision ID | Revision ID. | |
| 3 | RW | 0x00 | GPIO0 Output Value
|
Local GPIO Output Value. This value is output on the GPIO pin when the GPIO function is enabled, the local GPIO direction is set to output, and remote GPIO control is disabled.
0: Output LOW (default). 1: Output HIGH. |
|||
| 2:0 | RW | GPIO0 Mode | Determines operating mode for the GPIO pin:
x00: Functional input mode. x10: TRI-STATE™ 001: GPIO mode, output. 011: GPIO mode, input. 101: Remote-hold mode. The GPIO pin will be an output, and the value is received from the remote Deserializer. In remote-hold mode, data is maintained on link loss. 111: Remote-default mode. The GPIO pin will be an output, and the value is received from the remote Deserializer. In remote-default mode, GPIO's Output Value bit is output on link loss. |
||||
| 14 | 0x0E | GPIO1 and GPIO2 Configuration | 7 | RW | 0x00 | GPIO2 Output Value | Local GPIO Output Value. This value is output on the GPIO pin when the GPIO function is enabled, the local GPIO direction is set to output, and remote GPIO control is disabled.
0: Output LOW (default). 1: Output HIGH. |
| 6:4 | RW | GPIO2 Mode | Determines operating mode for the GPIO pin:
x00: Functional input mode. x10: TRI-STATE™. 001: GPIO mode, output. 011: GPIO mode, input. 101: Remote-hold mode. The GPIO pin will be an output, and the value is received from the remote Deserializer. In remote-hold mode, data is maintained on link loss. 111: Remote-default mode. The GPIO pin will be an output, and the value is received from the remote Deserializer. In remote-default mode, GPIO's Output Value bit is output on link loss. |
||||
| 3 | RW | GPIO1 Output Value | Local GPIO Output Value. This value is output on the GPIO pin when the GPIO function is enabled, the local GPIO direction is set to output, and remote GPIO control is disabled.
0: Output LOW (default). 1: Output HIGH. |
||||
| 2:0 | RW | GPIO1 Mode | Determines operating mode for the GPIO pin:
x00: Functional input mode. x10: TRI-STATE™. 001: GPIO mode, output. 011: GPIO mode, input. 101: Remote-hold mode. The GPIO pin will be an output, and the value is received from the remote Deserializer. In remote-hold mode, data is maintained on link loss. 111: Remote-default mode. The GPIO pin will be an output, and the value is received from the remote Deserializer. In remote-default mode, GPIO's Output Value bit is output on link loss. |
||||
| 15 | 0x0F | GPIO3 Configuration | 7:4 | 0x00 | Reserved. | ||
| 3 | RW | GPIO3 Output Value | Local GPIO Output Value. This value is output on the GPIO pin when the GPIO function is enabled, the local GPIO direction is set to output, and remote GPIO control is disabled.
0: Output LOW (default). 1: Output HIGH. |
||||
| 2:0 | RW | GPIO3 Mode | Determines operating mode for the GPIO pin:
x00: Functional input mode. x10: TRI-STATE. 001: GPIO mode, output. 011: GPIO mode, input. 101: Remote-hold mode. The GPIO pin will be an output, and the value is received from the remote Deserializer. In remote-hold mode, data is maintained on link loss. 111: Remote-default mode. The GPIO pin will be an output, and the value is received from the remote Deserializer. In remote-default mode, GPIO's Output Value bit is output on link loss. |
||||
| 16 | 0x10 | GPIO5_REG and GPIO6_REG Configuration | 7 | RW | 0x00 | GPIO6_REG Output Value | Local GPIO Output Value. This value is output on the GPIO pin when the GPIO function is enabled and the local GPIO direction is set to output.
0: Output LOW (default). 1: Output HIGH. |
| 6 | Reserved. | ||||||
| 5:4 | RW | GPIO6_REG Mode | Determines operating mode for the GPIO pin:
00: Functional input mode. 10: TRI-STATE™. 01: GPIO mode, output. 11: GPIO mode; input. |
||||
| 3 | RW | GPIO5_REG Output Value | Local GPIO Output Value. This value is output on the GPIO pin when the GPIO function is enabled and the local GPIO direction is set to output.
0: Output LOW (default). 1: Output HIGH. |
||||
| 2 | Reserved. | ||||||
| 1:0 | RW | GPIO5_REG Mode | Determines operating mode for the GPIO pin:
00: Functional input mode. 10: TRI-STATE™. 01: GPIO mode, output. 11: GPIO mode; input. |
||||
| 17 | 0x11 | GPIO7_REG and GPIO8_REG Configuration | 7 | RW | 0x00 | GPIO8_REG Output Value | Local GPIO Output Value. This value is output on the GPIO pin when the GPIO function is enabled and the local GPIO direction is set to output.
0: Output LOW (default). 1: Output HIGH. |
| 6 | Reserved. | ||||||
| 5:4 | RW | GPIO8_REG Mode | Determines operating mode for the GPIO pin:
00: Functional input mode. 10: TRI-STATE. 01: GPIO mode, output. 11: GPIO mode; input. |
||||
| 3 | RW | GPIO7_REG Output Value | Local GPIO Output Value. This value is output on the GPIO pin when the GPIO function is enabled and the local GPIO direction is set to output.
0: Output LOW (default). 1: Output HIGH. |
||||
| 2 | Reserved. | ||||||
| 1:0 | RW | GPIO7_REG Mode | Determines operating mode for the GPIO pin:
00: Functional input mode. 10: TRI-STATE. 01: GPIO mode, output. 11: GPIO mode; input. |
||||
| 18 | 0x12 | Data Path Control | 7 | 0x00 | Reserved. | ||
| 6 | RW | Pass RGB | Setting this bit causes RGB data to be sent independent of DE. However, setting this bit prevents HDCP operation and blocks packetized audio.
0: Normal operation. 1: Pass RGB independent of DE. |
||||
| 5 | RW | DE Polarity | This bit indicates the polarity of the DE (Data Enable) signal.
0: DE is positive (active high, idle low). 1: DE is inverted (active low, idle high). |
||||
| 4 | RW | I2S Repeater Regen | Regenerate I2S data from Repeater I2S pins.
0: Repeater pass through I2S from video pins (default). 1: Repeater regenerate I2S from I2S pins. |
||||
| 3 | RW | I2S Channel B Enable Override | I2S Channel B Enable Override.
0: Disable I2S Channel B override. 1: Set I2S Channel B Enable from 0x12[0]. |
||||
| 2 | RW | 18-Bit Video Select | 0: Select 24-bit video mode.
1: Select 18-bit video mode. |
||||
| 1 | RW | I2S Transport Select | Select I2S transport mode:
0: Enable I2S Data Island transport (default). 1: Enable I2S Data Forward Channel Frame transport. |
||||
| 0 | RW | I2S Channel B Enable | I2S Channel B Enable.
0: I2S Channel B disabled. 1: Enable I2S Channel B on B1 input. Note that in a repeater, this bit may be overridden by the in-band I2S mode detection. |
||||
| 19 | 0x13 | General Purpose Control | 7 | R | 0x88 | MODE_SEL1 Done | Indicates MODE_SEL1 value has stabilized and has been latched. |
| 6:4 | R | MODE_SEL1 Decode | Returns the 3-bit decode of the MODE_SEL1 pin. | ||||
| 3 | R | MODE_SEL0 Done | Indicates MODE_SEL0 value has stabilized and has been latched. | ||||
| 2:0 | R | MODE_SEL0 Decode | Returns the 3-bit decode of the MODE_SEL0 pin. | ||||
| 20 | 0x14 | BIST Control | 7:3 | 0x00 | Reserved. | ||
| 2:1 | RW | OSC Clock Source | Allows choosing different OSC clock frequencies for forward channel frame.
OSC clock frequency in functional mode when TMDS clock is not present and 0x03[2]=1: 00: 50 MHz oscillator. 01: 50 MHz oscillator. 10: 100 MHz oscillator. 11: 25 MHz oscillator. Clock source in BIST mode i.e. when 0x14[0]=1: 00: External pixel clock. 01: 33 MHz oscillator. 1x: 100 MHz oscillator. |
||||
| 0 | RW | BIST Enable | BIST control:
0: Disabled (default). 1: Enabled. |
||||
| 21 | 0x15 | I2C Voltage Select | 7:0 | RW | 0x01 | I2C Voltage Select | Selects 1.8 or 3.3V for the I2C_SDA and I2C_SCL pins. This register is loaded from the I2C_VSEL strap option from the SCLK pin at power-up. At power-up, a logic LOW will select 3.3V operation, while a logic HIGH (pull-up resistor attached) will select 1.8V signaling. Issuing either of the digital resets via register 0x01 will cause the I2C_VSEL value to be reset to 3.3V operation.
Reads of this register return the status of the I2C_VSEL control: 0: Select 1.8V signaling. 1: Select 3.3V signaling. This bit may be overwritten via register access or via eFuse program by writing an 8-bit value to this register: Write 0xb5 to set I2C_VSEL. Write 0xb6 to clear I2C_VSEL. |
| 22 | 0x16 | BCC Watchdog Control | 7:1 | RW | 0xFE | Timer Value | The watchdog timer allows termination of a control channel transaction if it fails to complete within a programmed amount of time. This field sets the Bidirectional Control Channel Watchdog Timeout value in units of 2 milliseconds. This field should not be set to 0. Set to 0x01. |
| 0 | RW | Timer Control | Disable Bidirectional Control Channel (BCC) Watchdog Timer:
0: Enable BCC Watchdog Timer operation (default). 1: Disable BCC Watchdog Timer operation. |
||||
| 23 | 0x17 | I2C Control | 7 | RW | 0x1E | I2C Pass All
|
0: Enable Forward Control Channel pass-through only of I2C accesses to I2C Slave IDs matching either the remote Deserializer Slave ID or the remote Slave ID (default).
1: Enable Forward Control Channel pass-through of all I2C accesses to I2C Slave IDs that do not match the Serializer I2C Slave ID. |
| 6:4 | RW | SDA Hold Time | Internal SDA hold time:
Configures the amount of internal hold time provided for the SDA input relative to the SCL input. Units are 40 nanoseconds. |
||||
| 3:0 | RW | I2C Filter Depth | Configures the maximum width of glitch pulses on the SCL and SDA inputs that will be rejected. Units are 5 nanoseconds. | ||||
| 24 | 0x18 | SCL High Time | 7:0 | RW | 0x7F | TX_SCL_HIGH | I2C Master SCL high time:
This field configures the high pulse width of the SCL output when the Serializer is the Master on the local I2C bus. Units are 40 ns for the nominal oscillator clock frequency. The default value is set to provide a minimum 5us SCL high time with the internal oscillator clock running at 26.25MHz rather than the nominal 25MHz. Delay includes 5 additional oscillator clock periods. Min_delay = 38.0952ns * (TX_SCL_HIGH + 5). |
| 25 | 0x19 | SCL Low Time | 7:0 | RW | 0x7F | TX_SCL_LOW | I2C Master SCL low time:
This field configures the low pulse width of the SCL output when the Serializer is the Master on the local I2C bus. This value is also used as the SDA setup time by the I2C Slave for providing data prior to releasing SCL during accesses over the Bidirectional Control Channel. Units are 40 ns for the nominal oscillator clock frequency. The default value is set to provide a minimum 5us SCL low time with the internal oscillator clock running at 26.25MHz rather than the nominal 25MHz. Delay includes 5 additional clock periods. Min_delay = 38.0952ns * (TX_SCL_LOW + 5). |
| 26 | 0x1A | Data Path Control 2 | 7:4 | Reserved. | |||
| 3 | R | Strap | SECONDARY_AUDIO | Enable Secondary Audio.
This register indicates that the AUX audio channel is enabled. The control for this function is via the AUX_AUDIO bit in the BRIDGE_CFG register register offset 0x54). The AUX_AUDIO control is strapped from the MODE_SEL0 pin at power-up. |
|||
| 2 | 0x01 | Reserved. | |||||
| 1 | RW | MODE_28B | Enable 28-bit Serializer Mode.
0: 24-bit high-speed data + 3 low-speed control (DE, HS, VS). 1: 28-bit high-speed data mode. |
||||
| 0 | RW | I2S Surround | Enable 5.1- or 7.1-channel I2S audio transport:
0: 2-channel or 4-channel I2S audio is enabled as configured in register 0x12 bits 3 and 0. 1: 5.1- or 7.1-channel audio is enabled. Note that I2S Data Island Transport is the only option for surround audio. Also note that in a repeater, this bit may be overridden by the in-band I2S mode detection (default). |
||||
| 27 | 0x1B | BIST BC Error Count | 7:0 | R | 0x00 | BIST BC Error
|
BIST back channel CRC error counter.
This register stores the back channel CRC error count during BIST Mode (saturates at 255 errors). Clears when a new BIST is initiated or by 0x04[5]. |
| 28 | 0x1C | GPIO Pin Status 1 | 7 | R | 0x00 | GPIO7_REG Pin Status | GPIO7_REG input pin status.
Note: status valid only if pin is set to GPI (input) mode. |
| 6 | R | GPIO6_REG Pin Status | GPIO6_REG input pin status.
Note: status valid only if pin is set to GPI (input) mode. |
||||
| 5 | R | GPIO5_REG Pin Status | GPIO5_REG input pin status.
Note: status valid only if pin is set to GPI (input) mode. |
||||
| 4 | Reserved. | ||||||
| 3 | R | GPIO3 Pin Status
|
GPIO3 input pin status.
Note: status valid only if pin is set to GPI (input) mode. |
||||
| 2 | R | GPIO2 Pin Status
|
GPIO2 input pin status.
Note: status valid only if pin is set to GPI (input) mode. |
||||
| 1 | R | GPIO1 Pin Status
|
GPIO1 input pin status.
Note: status valid only if pin is set to GPI (input) mode. |
||||
| 0 | R | GPIO0 Pin Status
|
GPIO0 input pin status.
Note: status valid only if pin is set to GPI (input) mode. |
||||
| 29 | 0x1D | GPIO Pin Status 2 | 7:1 | 0x00 | Reserved | ||
| 0 | R | GPIO8_REG Pin Status | GPIO8_REG input pin status.
Note: status valid only if pin is set to GPI (input) mode. |
||||
| 30 | 0x1E | Transmitter Port Select | 7:3 | Reserved. | |||
| 2 | RW | 0x01 | PORT1_I2C_EN | Port1 I2C Enable.
Enables secondary I2C address. The second I2C address provides access to Port1 registers as well as registers that are shared between Port0 and Port1. The second I2C address value will be set to DeviceID + 1 (7-bit format). The PORT1_I2C_EN bit must also be set to allow accessing remote devices over the second link when the device is in Replicate mode. |
|||
| 1 | RW | PORT1_SEL | Selects Port1 for register access from primary I2C address.
For writes, Port1 registers and shared registers will both be written. For reads, Port1 registers and shared registers will be read. This bit must be cleared to read Port0 registers. This bit is ignored if PORT1_I2C_EN is set. |
||||
| 0 | RW | PORT0_SEL | Selects Port0 for register access from primary I2C address.
For writes, Port0 registers and shared registers will both be written. For reads, Port0 registers and shared registers will be read. Note that if PORT1_SEL is also set, then Port1 registers will be read. This bit is ignored if PORT1_I2C_EN is set. |
||||
| 31 | 0x1F | Frequency Counter | 7:0 | RW | 0x00 | Frequency Count | Frequency counter control.
A write to this register will enable a frequency counter to count the number of pixel clock during a specified time interval. The time interval is equal to the value written multiplied by the oscillator clock period (nominally 40ns). A read of the register returns the number of pixel clock edges seen during the enabled interval. The frequency counter will freeze at 0xff if it reaches the maximum value. The frequency counter will provide a rough estimate of the pixel clock period. If the pixel clock frequency is known, the frequency counter may be used to determine the actual oscillator clock frequency. |
| 32 | 0x20 | Deserializer Capabilities 1 | 7 | RW | 0x00 | FREEZE_DES_CAP
|
Freeze Deserializer Capabilities.
Prevent auto-loading of the Deserializer Capabilities by the Bidirectional Control Channel. The Capabilities will be frozen at the values written in registers 0x20 and 0x21. |
| 6 |
|
Reserved. | |||||
| 5 | SEND_FREQ
|
Send Frequency Training Pattern.
Indicates the DS90UH929-Q1 should send the Frequency Training Pattern. This field is automatically configured by the Bidirectional Control Channel once RX Lock has been detected. Software may overwrite this value, but must also set the FREEZE DES CAP bit to prevent overwriting by the Bidirectional Control Channel. |
|||||
| 4 | RW | 0x00 | SEND_EQ
|
Send Equalization Training Pattern.
Indicates the DS90UH929-Q1 should send the Equalization Training Pattern. This field is automatically configured by the Bidirectional Control Channel once RX Lock has been detected. Software may overwrite this value, but must also set the FREEZE DES CAP bit to prevent overwriting by the Bidirectional Control Channel. |
|||
| 3 | RW | DUAL_LINK_CAP
|
Dual link Capabilities.
Indicates if the Deserializer is capable of dual link operation. This field is automatically configured by the Bidirectional Control Channel once RX Lock has been detected. Software may overwrite this value, but must also set the FREEZE DES CAP bit to prevent overwriting by the Bidirectional Control Channel. |
||||
| 2 | RW | DUAL_CHANNEL
|
Dual Channel 0/1 Indication.
In a dual-link capable device, indicates if this is the primary or secondary channel. 0: Primary channel (channel 0). 1: Secondary channel (channel 1). This field is automatically configured by the Bidirectional Control Channel once RX Lock has been detected. Software may overwrite this value, but must also set the FREEZE DES CAP bit to prevent overwriting by the Bidirectional Control Channel. |
||||
| 32 | 0x20 | Deserializer Capabilities 1 | 1 | RW | 0x00 | VID_24B_HD_AUD
|
Deserializer supports 24-bit video concurrently with HD audio.
This field is automatically configured by the Bidirectional Control Channel once RX Lock has been detected. Software may overwrite this value, but must also set the FREEZE DES CAP bit to prevent overwriting by the Bidirectional Control Channel. |
| 0 | RW | DES_CAP_FC_GPIO
|
Deserializer supports GPIO in the Forward Channel Frame.
This field is automatically configured by the Bidirectional Control Channel once RX Lock has been detected. Software may overwrite this value, but must also set the FREEZE DES CAP bit to prevent overwriting by the Bidirectional Control Channel. |
||||
| 33 | 0x21 | Deserializer Capabilities 2 | 7:2 | Reserved. | |||
| 1:0 |
|
Reserved. | |||||
| 38 | 0x26 | Link Detect Control | 7:3 | Reserved. | |||
| 2:0 | RW | 0x00 | LINK DETECT TIMER | Bidirectional Control Channel Link Detect Timer.
This field configures the link detection timeout period. If the timer expires without valid communication over the reverse channel, link detect will be deasserted. 000: 162 microseconds. 001: 325 microseconds. 010: 650 microseconds. 011: 1.3 milliseconds. 100: 10.25 microseconds. 101: 20.5 microseconds. 110: 41 microseconds. 111: 82 microseconds. |
|||
| 48 | 0x30 | SCLK_CTRL | 7 | RW | 0x00 | SCLK/WS | SCLK to Word Select Ratio.
0 : 64. 1 : 32. |
| 6:5 | RW | MCLK/SCLK | MCLK to SCLK Select Ratio.
00 : 4. 01 : 2. 10 : 1. 11 : 8. |
||||
| 4:3 | RW | CLEAN CLOCK_DIV | Clock Cleaner divider.
00 : FPD_VCO_CLOCK/8. 01 : FPD_VCO_CLOCK/4. 10 : FPD_VCO_CLOCK/2. 11 : AON_OSC. |
||||
| 2:1 | RW | CLEAN Mode | If non-zero, the SCLK Input or HDMI N/CTS generated Audio Clock is cleaned digitally before being used.
00 : Off. 01 : ratio of 1. 10 : ratio of 2. 11 : ratio of 4. |
||||
| 0 | RW | MASTER | If set, the SCLK I/O and the WS_IO are used as an output and the Clock Generation Circuits are enabled, otherwise they are inputs. | ||||
| 49 | 0x31 | AUDIO_CTS0 | 7:0 | RW | 0x00 | CTS[7:0] | If non-zero, the CTS value is used to generate a new clock from the PFD PLLs VCO. |
| 50 | 0x32 | AUDIO_CTS1 | 7:0 | RW | 0x00 | CTS[15:8] | If non-zero, the CTS value is used to generate a new clock from the PFD PLLs VCO. |
| 51 | 0x33 | AUDIO_CTS2 | 7:0 | RW | 0x00 | CTS[23:16] | If non-zero, the CTS value is used to generate a new clock from the PFD PLLs VCO. |
| 52 | 0x34 | AUDIO_N0 | 7:0 | RW | 0x00 | N[7:0] | If non-zero, the CTS value is used to generate a new clock from the PFD PLLs VCO. |
| 53 | 0x35 | AUDIO_N1 | 7:0 | RW | 0x00 | N[15:8] | If non-zero, the CTS value is used to generate a new clock from the PFD PLLs VCO. |
| 54 | 0x36 | AUDIO_N2_COEFF | 7:4 | RW | 0x00 | COEFF[3:0] | Selects the LPF_COEFF in the Clock Cleaner (Feedback is divided by 2^COEFF). |
| 3:0 | RW | 0x00 | N[19:16] | If non-zero, the CTS value is used to generate a new clock from the PFD PLLs VCO. | |||
| 55 | 0x37 | CLK_CLEAN_STS | 7:6 | Reserved. | |||
| 5:3 | R | 0x00 | IN_FIFO_LVL | Clock Cleaner Input FIFO Level. | |||
| 2:0 | R | 0x00 | OUT_FIFO_LVL | Clock Cleaner Output FIFO Level. | |||
| 64 | 0x40 | ANA_IA_CNTL | 7:5 | 0x00 | Reserved. | ||
| 4:2 | RW | ANA_IA_SEL | Analog register select
Selects target for register access 000b: Disabled 001b - 011b: Reserved 100b: HDMI Registers 101b: FPD3 TX Registers 11xb: Reserved |
||||
| 1 | RW | ANA_AUTO_INC | Analog Register Auto Increment
0: Disable auto-increment mode 1: Enable auto-increment mode. Upon completion of a read or write, the register address will automatically be incremented by 1. |
||||
| 0 | RW | ANA_IA_READ | Start Analog Register Read
0: Write analog register 1: Read analog register |
||||
| 65 | 0x41 | ANA_IA_ADDR | 7:0 | RW | 0x00 | ANA_IA_ADDR | Analog register offset
This register contains the 8-bit register offset for the indirect access. |
| 66 | 0x42 | ANA_IA_DATA | 7:0 | RW | 0x00 | ANA_IA_DATA | Analog register data
Writing this register will cause an indirect write of the ANA_IA_DATA value to the selected analog block register. Reading this register will return the value of the selected analog block register. |
| 72 | 0x48 | APB_CTL | 7:5 | Reserved. | |||
| 4:3 | RW | 0x00 | APB_SELECT | APB Select: Selects target for register access.
00 : HDMI APB interface. 01 : EDID SRAM. 10 : Configuration Data (read only). 11 : Die ID (read only). |
|||
| 2 | RW | APB_AUTO_INC | APB Auto Increment: Enables auto-increment mode. Upon completion of an APB read or write, the APB address will automatically be incremented by 0x4 for HDMI registers or by 0x1 for others. | ||||
| 1 | RW | APB_READ | Start APB Read: Setting this bit to a 1 will begin an APB read. Read data will be available in the APB_DATAx registers. The APB_ADRx registers should be programmed prior to setting this bit. This bit will be cleared when the read is complete. | ||||
| 0 | RW | APB_ENABLE | APB Interface Enable: Set to a 1 to enable the APB interface. The APB_SELECT bits indicate what device is selected. | ||||
| 73 | 0x49 | APB_ADR0 | 7:0 | RW | 0x00 | APB_ADR0 | APB Address byte 0 (LSB). |
| 74 | 0x4A | APB_ADR1 | 7:0 | RW | 0x00 | APB_ADR1 | APB Address byte 1 (MSB). |
| 75 | 0x4B | APB_DATA0 | 7:0 | RW | 0x00 | APB_DATA0 | Byte 0 (LSB) of the APB Interface Data. |
| 76 | 0x4C | APB_DATA1 | 7:0 | RW | 0x00 | APB_DATA1 | Byte 1 of the APB Interface Data. |
| 77 | 0x4D | APB_DATA2 | 7:0 | RW | 0x00 | APB_DATA2 | Byte 2 of the APB Interface Data. |
| 78 | 0x4E | APB_DATA3 | 7:0 | RW | 0x00 | APB_DATA3 | Byte 3 (MSB) of the APB Interface Data. |
| 79 | 0x4F | BRIDGE_CTL | 7:5 | Reserved. | |||
| 4 | RW | 0x00 | CEC_CLK_SRC | CEC Clock Source Select: Selects clock source for generating the 32.768kHz clock for CEC operations in the HDMI Receive Controller.
0 : Selects internal generated clock. 1 : Selects external 25MHz oscillator clock. |
|||
| 3 | RW | CEC_CLK_EN | CEC Clock Enable: Enable CEC clock generation. Enables generation of the 32.768kHz clock for the HDMI Receive controller. This bit should be set prior to enabling CEC operation via the HDMI controller registers. | ||||
| 2 | RW | EDID_CLEAR | Clear EDID SRAM: Set to 1 to enable clearing the EDID SRAM. The EDID_INIT bit must be set at the same time for the clear to occur. This bit will be cleared when the initialization is complete. | ||||
| 1 | RW | EDID_INIT | Initialize EDID SRAM from EEPROM: Causes a reload of the EDID SRAM from the non-volatile EDID EEPROM. This bit will be cleared when the initialization is complete. | ||||
| 0 | R | Strap | EDID_DISABLE | Disable EDID access via DDC/I2C: Disables access to the EDID SRAM via the HDMI DDC interface. This value is loaded from the MODE_SEL0 pin at power-up. | |||
| 80 | 0x50 | BRIDGE_STS | 7 | R | 0x03 | RX5V_DETECT | RX +5V detect: Indicates status of the RX_5V pin. When asserted, indicates the HDMI interface has detected valid voltage on the RX_5V input. |
| 6 | R | HDMI_INT | HDMI Interrupt Status: Indicates an HDMI Interrupt is pending. HDMI interrupts are serviced through the HDMI Registers via the APB Interface. | ||||
| 5 | R | HDCP_INT | HDCP Interrupt Status: Indicates an HDCP Transmitter Interrupt is pending. HDCP Transmit interrupts are serviced through the HDCP Interrupt Control and Status registers. | ||||
| 4 | R | INIT_DONE | Initialization Done: Initialization sequence has completed. This step will complete after configuration complete (CFG_DONE). | ||||
| 3 | R | REM_EDID_LOAD | Remote EDID Loaded: Indicates EDID SRAM has been loaded from a remote EDID EEPROM device over the Bidirectional Control Channel. The EDID_CKSUM value indicates if the EDID load was successful. | ||||
| 2 | R | CFG_DONE | Configuration Complete: Indicates automatic configuration has completed. This step will complete prior to initialization complete (INIT_DONE). | ||||
| 1 | R | CFG_CKSUM | Configuration checksum status: Indicates result of Configuration checksum during initialization. The device verifies the 2’s complement checksum in the last 128 bytes of the EEPROM. A value of 1 indicates the checksum passed. | ||||
| 0 | R | EDID_CKSUM | EDID checksum Status: Indicates result of EDID checksum during EDID initialization. The device verifies the 2’s complement checksum in the first 256 bytes of the EEPROM. A value of 1 indicates the checksum passed. | ||||
| 81 | 0x51 | EDID_ID | 7:1 | RW | 0x50 | EDID_ID | EDID I2C Slave Address: I2C address used for accessing the EDID information. These are the upper 7 bits in 8-bit format addressing, where the lowest bit is the Read/Write control. |
| 0 | RW | 0 | EDID_RDONLY | EDID Read Only: Set to a 1 puts the EDID SRAM memory in read-only mode for access via the HDMI DDC interface. Setting to a 0 allows writes to the EDID SRAM memory. | |||
| 82 | 0x52 | EDID_CFG0 | 7 | Reserved. | |||
| 6:4 | RW | 0x01 | EDID_SDA_HOLD | Internal SDA Hold Time: This field configures the amount of internal hold time provided for the DDC_SDA input relative to the DDC_SCL input. Units are 40 nanoseconds. The hold time is used to qualify the start detection to avoid false detection of Start or Stop conditions. | |||
| 3:0 | RW | 0x0E | EDID_FLTR_DPTH | I2C Glitch Filter Depth: This field configures the maximum width of glitch pulses on the DDC_SCL and DDC_SDA inputs that will be rejected. Units are 5 nanoseconds. | |||
| 83 | 0x53 | EDID_CFG1 | 7:2 | Reserved. | |||
| 1:0 | RW | 0x00 | EDID_SDA_DLY | SDA Output Delay: This field configures output delay on the DDC_SDA output when the EDID memory is accessed. Setting this value will increase output delay in units of 40ns. Nominal output delay values for DDC_SCL to DDC_SDA are:
00 : 240ns. 01 : 280ns. 10 : 320ns. 11 : 360ns. |
|||
| 84 | 0x54 | BRIDGE_CFG | 7 | RW | Strap | EXT_CTL | External Control: When this bit Is set, the internal bridge control function is disabled. This disables initialization of the HDMI Receiver as well as initiation of HDCP functions. These operations must be controlled by an external controller attached to the I2C interface. This value is loaded from the MODE_SEL1 pin at power-up. |
| 6 | RW | 0x00 | HDMI_INT_EN | HDMI Interrupt Enable: When this bit is set, Interrupts from the HDMI Receive controller will be reported on the INTB pin. Software may check the BRIDGE_STS register to determine if the interrupt is from the HDMI Receiver or the HDCP Transmitter. | |||
| 5 | RW | Strap | DIS_REM_EDID | Disable Remote EDID load: Disables automatic load of EDID SRAM from a remote EDID EEPROM. By default, the device will check the remote I2C bus for an EEPROM with a valid EDID, and load the EDID data to local EDID SRAM. If this bit is set to a 1, the remote EDID load will be bypassed. This value is loaded from the MODE_SEL1 pin at power-up. | |||
| 4 | RW | 0x00 | AUTO_INIT_DIS | Disable Automatic initialization: The Bridge control will automatically initialize the HDMI Receiver for operation. Setting this bit to a 1 will disable automatic initialization of the HDMI Receiver. In this mode, initialization of the HDMI Receiver must be done through EEPROM configuration or via external control. | |||
| 3 | RW | 0x00 | AUTO_HDCP_DIS | Disable Automatic HDCP_CTRL setting: By default the internal bridge control function will configure the HDMI Receiver for HDCP operation using default settings for bits in the HDCP_CTRL register. Setting this bit to a 1 will disable automatic control of the HDCP_CTRL register in the HDMI Receiver. | |||
| 2 | RW | 0x00 | AUDIO_TDM | Enable TDM Audio: Setting this bit to a 1 will enable TDM audio for the HDMI audio. | |||
| 1 | RW | AUDIO_MODE | Audio Mode: Selects source for audio to be sent over the FPD-Link III downstream link.
0 : HDMI audio. 1 : Local/DVI audio. Local audio is sourced from the device I2S pins rather than from HDMI, and is useful in modes such as DVI that do not include audio. |
||||
| 0 | RW | Strap | AUX_AUDIO_EN | AUX Audio Channel Enable: Setting this bit to a 1 will enable the AUX audio channel. This allows sending additional 2-channel audio in addition to the HDMI or DVI audio. This bit is loaded from the MODE_SEL0 pin at power-up. | |||
| 85 | 0x55 | AUDIO_CFG | 7 | RW | 0x00 | TDM_2_PARALLEL | Enable I2S TDM to parallel audio conversion: When this bit is set, the i2s tdm to parallel conversion module is enabled. The clock output from the i2s tdm to parallel conversion module is them used to send data to the deserializer. |
| 6 | RW | HDMI_I2S_OUT | HDMI Audio Output Enable: When this bit is set, the HDMI I2S audio data will be output on the I2S audio interface pins. This control is ignored if the BRIDGE_CFG:AUDIO_MODE is not set to 00 (HDMI audio only). | ||||
| 5:4 | Reserved. | ||||||
| 3 | RW | 0x0C | RST_ON_TYPE | Reset Audio FIFO on Type Change: When this bit is set, the internal bridge control function will reset the HDMI Audio FIFO on a change in the Audio type. | |||
| 2 | RW | RST_ON_AIF | Reset Audio FIFO on Audio Infoframe: When this bit is set, the internal bridge control function will reset the HDMI Audio FIFO on a change in the Audio Infoframe checksum. | ||||
| 1 | RW | RST_ON_AVI | Reset Audio FIFO on Audio Video Information Infoframe: When this bit is set, the internal bridge control function will reset the HDMI Audio FIFO on a change in the Audio Video Information Infoframe checksum. | ||||
| 0 | RW | RST_ON_ACR | Reset Audio FIFO on Audio Control Frame: When this bit is set, the internal bridge control function will reset the HDMI Audio FIFO on a change in the Audio Control Frame N or CTS fields. | ||||
| 90 | 0x5A | FPD3_STS | 7 | R | 0x00 | FPD3_LINK_RDY | This bit indicates that the FPD-Link III has detected a valid downstream connection and determined capabilities for the downstream link. |
| 6 | R | FPD3_TX_STS | FPD-Link III transmit status:
This bit indicates that the FPD-Link III transmitter is active and the receiver is LOCKED to the transmit clock. It is only asserted once a valid input has been detected, and the FPD-Link III transmit connection has entered the correct mode (Single vs. Dual mode). |
||||
| 5:4 | R | FPD3_PORT_STS | FPD3 Port Status: If FPD3_TX_STS is set to a 1, this field indicates the port mode status as follows:
01: Single FPD-Link III Transmit on port 0. |
||||
| 3 | R | TMDS_VALID | HDMI TMDS Valid: This bit indicates the TMDS interface is recovering valid TMDS data from HDMI. | ||||
| 2 | R | HDMI_PLL_LOCK | HDMI PLL lock status: Indicates the HDMI PLL has locked to the incoming TMDS clock. | ||||
| 1 | R | NO_HDMI_CLK | No TMDS Clock Detected: This bit indicates the Frequency Detect circuit did not detect an TMDS clock greater than the value specified in the FREQ_LOW register. | ||||
| 0 | R | FREQ_STABLE | HDMI Frequency is Stable: Indicates the Frequency Detection circuit has detected a stable TMDS clock frequency. | ||||
| 91 | 0x5B | FPD3_CTL1 | 7 | RW | Strap | FPD3_COAX_MODE | FPD3 Coax Mode: Enables configuration for the FPD3 Interface cabling type.
0 : Twisted Pair. 1 : Coax This bit is loaded from the MODE_SEL1 pin at power-up. |
| 6 | Reserved. | ||||||
| 5 | RW | 1 | RST_PLL_FREQ | Reset FPD3 PLL on Frequency Change: When set to a 1, frequency changes detected by the Frequency Detect circuit will result in a reset of the FPD3 PLL. Set to 0. | |||
| 4 | RW | 0 | FREQ_DET_PLL | Frequency Detect Select PLL Clock: Determines the clock source for the Frequency detection circuit:
0 : TMDS clock (prior to PLL). 1: HDMI PLL clock. |
|||
| 3 | Reserved. | ||||||
| 2 | Reserved. | ||||||
| 1 | Reserved. | ||||||
| 0 | Reserved. | ||||||
| 92 | 0x5C | FPD3_CTL2 | 7 | Reserved. | |||
| 6 | RW | 0x00 | FORCE_LINK_RDY | Force Link Ready: Forces link ready indication, bypassing back channel link detection. | |||
| 5 | RW | FORCE_CLK_DET | Force Clock Detect: Forces the HDMI/OpenLDI clock detect circuit to indicate presence of a valid input clock. This bypasses the clock detect circuit, allowing operation with an input clock that does not meet frequency or stability requirements. | ||||
| 4:3 | RW | FREQ_STBL_THR | Frequency Stability Threshold: The Frequency detect circuit can be used to detect a stable clock frequency. The Stability Threshold determines the amount of time required for the clock frequency to stay within the FREQ_HYST range to be considered stable:
00 : 40us. 01 : 80us. 10 : 320us. 11 : 1.28ms. |
||||
| 2:0 | RW | 0x02 | FREQ_HYST | Frequency Detect Hysteresis: The Frequency detect hysteresis setting allows ignoring minor fluctuations in frequency. A new frequency measurement will be captured only if the measured frequency differs from the current measured frequency by more than the FREQ_HYST setting. The FREQ_HYST setting is in MHz. | |||
| 93 | 0x5D | FREQ_LOW | 7 | Reserved. | |||
| 6 | RW | 0 | HDMI_RST_MODE | HDMI Phy Reset Mode:
0 : Reset HDMI Phy on change in mode or frequency. 1 : Don't reset HDMI Phy on change in mode or frequency if +5 V is asserted. |
|||
| 5:0 | RW | 6 | FREQ_LO_THR | Frequency Low Threshold: Sets the low threshold for the TMDS Clock frequency detect circuit in MHz. This value is used to determine if the TMDS clock frequency is too low for proper operation. | |||
| 95 | 0x5F | HDMI Frequency | 7:0 | R | 0x00 | HDMI_FREQ | HDMI frequency:
Returns the value of the HDMI frequency in MHz. A value of 0 indicates the HDMI receiver is not detecting a valid signal. |
| 100 | 0x64 | Pattern Generator Control | 7:4 | RW | 0x10 | Pattern Generator Select | Fixed Pattern Select
Selects the pattern to output when in Fixed Pattern Mode. Scaled patterns are evenly distributed across the horizontal or vertical active regions. This field is ignored when Auto-Scrolling Mode is enabled. xxxx: normal/inverted. 0000: Checkerboard. 0001: White/Black (default). 0010: Black/White. 0011: Red/Cyan. 0100: Green/Magenta. 0101: Blue/Yellow. 0110: Horizontal Black-White/White-Black. 0111: Horizontal Black-Red/White-Cyan. 1000: Horizontal Black-Green/White-Magenta. 1001: Horizontal Black-Blue/White-Yellow. 1010: Vertical Black-White/White-Black. 1011: Vertical Black-Red/White-Cyan. 1100: Vertical Black-Green/White-Magenta. 1101: Vertical Black-Blue/White-Yellow. 1110: Custom color (or its inversion) configured in PGRS, PGGS, PGBS registers. 1111: VCOM. See TI App Note AN-2198. |
| 3 | Reserved. | ||||||
| 2 | RW | Color Bars Pattern | Enable color bars:
0: Color Bars disabled (default). 1: Color Bars enabled. Overrides the selection from reg_0x64[7:4]. |
||||
| 1 | RW | VCOM Pattern Reverse | Reverse order of color bands in VCOM pattern:
0: Color sequence from top left is (YCBR) (default). 1: Color sequence from top left is (RBCY). |
||||
| 0 | RW | Pattern Generator Enable | Pattern Generator enable:
0: Disable Pattern Generator (default). 1: Enable Pattern Generator. |
||||
| 101 | 0x65 | Pattern Generator Configuration | 7 | 0x00 | Reserved. | ||
| 6 | RW | Checkerboard Scale | Scale Checkered Patterns:
0: Normal operation (each square is 1x1 pixel) (default). 1: Scale checkered patterns (VCOM and checkerboard) by 8 (each square is 8x8 pixels). Setting this bit gives better visibility of the checkered patterns. |
||||
| 5 | RW | Custom Checkerboard | Use Custom Checkerboard Color:
0: Use white and black in the Checkerboard pattern (default). 1: Use the Custom Color and black in the Checkerboard pattern. |
||||
| 4 | RW | PG 18–bit Mode | 18-bit Mode Select:
0: Enable 24-bit pattern generation. Scaled patterns use 256 levels of brightness (default). 1: Enable 18-bit color pattern generation. Scaled patterns will have 64 levels of brightness and the R, G, and B outputs use the six most significant color bits. |
||||
| 3 | RW | External Clock | Select External Clock Source:
0: Selects the internal divided clock when using internal timing (default). 1: Selects the external pixel clock when using internal timing. This bit has no effect in external timing mode (PATGEN_TSEL = 0). |
||||
| 2 | RW | Timing Select | Timing Select Control:
0: The Pattern Generator uses external video timing from the pixel clock, Data Enable, Horizontal Sync, and Vertical Sync signals (default). 1: The Pattern Generator creates its own video timing as configured in the Pattern Generator Total Frame Size, Active Frame Size. Horizontal Sync Width, Vertical Sync Width, Horizontal Back Porch, Vertical Back Porch, and Sync Configuration registers. See Exploring the Internal Test Pattern Generation Feature of 720p FPD-Link III Devices (SNLA132). |
||||
| 1 | RW | Color Invert | Enable Inverted Color Patterns:
0: Do not invert the color output (default). 1: Invert the color output. See Exploring the Internal Test Pattern Generation Feature of 720p FPD-Link III Devices (SNLA132). |
||||
| 0 | RW | Auto Scroll | Auto Scroll Enable:
0: The Pattern Generator retains the current pattern (default). 1: The Pattern Generator will automatically move to the next enabled pattern after the number of frames specified in the Pattern Generator Frame Time (PGFT) register. See Exploring the Internal Test Pattern Generation Feature of 720p FPD-Link III Devices (SNLA132). |
||||
| 102 | 0x66 | PGIA | 7:0 | RW | 0x00 | PG Indirect Address | This 8-bit field sets the indirect address for accesses to indirectly-mapped registers. It should be written prior to reading or writing the Pattern Generator Indirect Data register.
See Exploring the Internal Test Pattern Generation Feature of 720p FPD-Link III Devices (SNLA132). |
| 103 | 0x67 | PGID | 7:0 | RW | 0x00 | PG Indirect Data | When writing to indirect registers, this register contains the data to be written. When reading from indirect registers, this register contains the read back value.
See Exploring the Internal Test Pattern Generation Feature of 720p FPD-Link III Devices (SNLA132). |
| 112 | 0x70 | Slave ID[1] | 7:1 | RW | 0x00 | Slave ID 1
|
7-bit I2C address of the remote Slave 1 attached to the remote Deserializer. If an I2C transaction is addressed to Slave Alias ID 1, the transaction will be remapped to this address before passing the transaction across the Bidirectional Control Channel to the Deserializer. A value of 0 in this field disables access to the remote Slave 1.
|
| 0 | Reserved. | ||||||
| 113 | 0x71 | Slave ID[2] | 7:1 | RW | 0x00 | Slave ID 2
|
7-bit I2C address of the remote Slave 2 attached to the remote Deserializer. If an I2C transaction is addressed to Slave Alias ID 2, the transaction will be remapped to this address before passing the transaction across the Bidirectional Control Channel to the Deserializer. A value of 0 in this field disables access to the remote Slave 2.
|
| 0 | Reserved. | ||||||
| 114 | 0x72 | Slave ID[3] | 7:1 | RW | 0x00 | Slave ID 3
|
7-bit I2C address of the remote Slave 3 attached to the remote Deserializer. If an I2C transaction is addressed to Slave Alias ID 3, the transaction will be remapped to this address before passing the transaction across the Bidirectional Control Channel to the Deserializer. A value of 0 in this field disables access to the remote Slave 3.
|
| 0 | Reserved. | ||||||
| 115 | 0x73 | Slave ID[4] | 7:1 | RW | 0x00 | Slave ID 4
|
7-bit I2C address of the remote Slave 4 attached to the remote Deserializer. If an I2C transaction is addressed to Slave Alias ID 4, the transaction will be remapped to this address before passing the transaction across the Bidirectional Control Channel to the Deserializer. A value of 0 in this field disables access to the remote Slave 4.
|
| 0 | Reserved. | ||||||
| 116 | 0x74 | Slave ID[5] | 7:1 | RW | 0x00 | Slave ID 5
|
7-bit I2C address of the remote Slave 5 attached to the remote Deserializer. If an I2C transaction is addressed to Slave Alias ID 5, the transaction will be remapped to this address before passing the transaction across the Bidirectional Control Channel to the Deserializer. A value of 0 in this field disables access to the remote Slave 5.
|
| 0 | Reserved. | ||||||
| 117 | 0x75 | Slave ID[6] | 7:1 | RW | 0x00 | Slave ID 6
|
7-bit I2C address of the remote Slave 6 attached to the remote Deserializer. If an I2C transaction is addressed to Slave Alias ID 6, the transaction will be remapped to this address before passing the transaction across the Bidirectional Control Channel to the Deserializer. A value of 0 in this field disables access to the remote Slave 6.
|
| 0 | Reserved. | ||||||
| 118 | 0x76 | Slave ID[7] | 7:1 | RW | 0x00 | Slave ID 7
|
7-bit I2C address of the remote Slave 7 attached to the remote Deserializer. If an I2C transaction is addressed to Slave Alias ID 7, the transaction will be remapped to this address before passing the transaction across the Bidirectional Control Channel to the Deserializer. A value of 0 in this field disables access to the remote Slave 7.
|
| 0 | Reserved. | ||||||
| 119 | 0x77 | Slave Alias[1] | 7:1 | RW | 0x00 | Slave Alias ID 1
|
7-bit Slave Alias ID of the remote Slave 1 attached to the remote Deserializer. The transaction will be remapped to the address specified in the Slave ID 1 register. A value of 0 in this field disables access to the remote Slave 1.
|
| 0 | Reserved. | ||||||
| 120 | 0x78 | Slave Alias[2] | 7:1 | RW | 0x00 | Slave Alias ID 2
|
7-bit Slave Alias ID of the remote Slave 2 attached to the remote Deserializer. The transaction will be remapped to the address specified in the Slave ID 2 register. A value of 0 in this field disables access to the remote Slave 2.
|
| 0 | Reserved. | ||||||
| 121 | 0x79 | Slave Alias[3] | 7:1 | RW | 0x00 | Slave Alias ID 3
|
7-bit Slave Alias ID of the remote Slave 3 attached to the remote Deserializer. The transaction will be remapped to the address specified in the Slave ID 3 register. A value of 0 in this field disables access to the remote Slave 3.
|
| 0 | Reserved. | ||||||
| 122 | 0x7A | Slave Alias[4] | 7:1 | RW | 0x00 | Slave Alias ID 4
|
7-bit Slave Alias ID of the remote Slave 4 attached to the remote Deserializer. The transaction will be remapped to the address specified in the Slave ID 4 register. A value of 0 in this field disables access to the remote Slave 4.
|
| 0 | Reserved. | ||||||
| 123 | 0x7B | Slave Alias[5] | 7:1 | RW | 0x00 | Slave Alias ID 5
|
7-bit Slave Alias ID of the remote Slave 5 attached to the remote Deserializer. The transaction will be remapped to the address specified in the Slave ID 5 register. A value of 0 in this field disables access to the remote Slave 5.
|
| 0 | Reserved. | ||||||
| 124 | 0x7C | Slave Alias[6] | 7:1 | RW | 0x00 | Slave Alias ID 6
|
7-bit Slave Alias ID of the remote Slave 6 attached to the remote Deserializer. The transaction will be remapped to the address specified in the Slave ID 6 register. A value of 0 in this field disables access to the remote Slave 6.
|
| 0 | Reserved. | ||||||
| 125 | 0x7D | Slave Alias[7] | 7:1 | RW | 0x00 | Slave Alias ID 7
|
7-bit Slave Alias ID of the remote Slave 7 attached to the remote Deserializer. The transaction will be remapped to the address specified in the Slave ID 7 register. A value of 0 in this field disables access to the remote Slave 7.
|
| 0 | Reserved. | ||||||
| 128 | 0x80 | RX_BKSV0 | 7:0 | R | 0x00 | RX_BKSV0 | BKSV0: Value of byte0 of the Receiver KSV. |
| 129 | 0x81 | RX_BKSV1 | 7:0 | R | 0x00 | RX_BKSV1 | BKSV1: Value of byte1 of the Receiver KSV. |
| 130 | 0x82 | RX_BKSV2 | 7:0 | R | 0x00 | RX_BKSV2 | BKSV2: Value of byte2 of the Receiver KSV. |
| 131 | 0x83 | RX_BKSV3 | 7:0 | R | 0x00 | RX_BKSV3 | BKSV3: Value of byte3 of the Receiver KSV. |
| 132 | 0x84 | RX_BKSV4 | 7:0 | R | 0x00 | RX_BKSV4 | BKSV4: Value of byte4 of the Receiver KSV. |
| 144 | 0x90 | TX_KSV0 | 7:0 | R | 0x00 | TX_KSV0 | TX_KSV0: Value of byte0 of the Transmitter KSV. |
| 145 | 0x91 | TX_KSV1 | 7:0 | R | 0x00 | TX_KSV1 | TX_KSV1: Value of byte1 of the Transmitter KSV. |
| 146 | 0x92 | TX_KSV2 | 7:0 | R | 0x00 | TX_KSV2 | TX_KSV2: Value of byte2 of the Transmitter KSV. |
| 147 | 0x93 | TX_KSV3 | 7:0 | R | 0x00 | TX_KSV3 | TX_KSV3: Value of byte3 of the Transmitter KSV. |
| 148 | 0x94 | TX_KSV4 | 7:0 | R | 0x00 | TX_KSV4 | TX_KSV4: Value of byte4 of the Transmitter KSV. |
| 160 | 0xA0 | RX_BCAPS | 7 | Reserved. | |||
| 6 | R | 0x01 | Repeater | Repeater: Indicates if the attached Receiver supports downstream connections. This bit is valid once the Bksv is ready as indicated by the BKSV_RDY bit in the HDCP. | |||
| 5 | R | KSV_FIFO_RDY | KSV FIFO Ready: Indicates the receiver has built the list of attached KSVs and computed the verification value V’. | ||||
| 4 | R | FAST_I2C | Fast I2C: The HDCP Receiver supports fast I2C. Since the I2C is embedded in the serial data, this bit is not relevant. | ||||
| 3:2 | Reserved. | ||||||
| 1 | R | 0x03 | FEATURES_1_1 | 1.1_Features: The HDCP Receiver supports the Enhanced Encryption Status Signaling (EESS), Advance Cipher, and Enhanced Link Verification options. | |||
| 0 | R | FAST_REAUTH | Fast Reauthentication: The HDCP Receiver is capable of receiving (unencrypted) video signal during the session re-authentication. | ||||
| 161 | 0xA1 | RX_BSTATUS0 | 7 | R | 0x00 | MAX_DEVS_EXCEEDED | Maximum Devices Exceeded: Indicates a topology error was detected. Indicates the number of downstream devices has exceeded the depth of the Repeater's KSV FIFO. |
| 6:0 | R | DEVICE_COUNT | Device Count: Total number of attached downstream device. For a Repeater, this will indicate the number of downstream devices, not including the Repeater. For an HDCP Receiver that is not also a Repeater, this field will be 0. | ||||
| 162 | 0xA2 | RX_BSTATUS1 | 7:4 | Reserved. | |||
| 3 | R | 0x00 | MAX_CASC_EXCEEDED | Maximum Cascade Exceeded: Indicates a topology error was detected. Indicates that more than seven levels of repeaters have been cascaded together. | |||
| 2:0 | R | Cascade Depth | Cascade Depth: Indicates the number of attached levels of devices for the Repeater. | ||||
| 163 | 0xA3 | KSV_FIFO | 7:0 | R | 0x00 | KSV_FIFO | KSV FIFO: Each read of the KSV FIFO returns one byte of the KSV FIFO list composed by the downstream Receiver. |
| 192 | 0xC0 | HDCP_DBG | 7 | Reserved. | |||
| 6 | RW | 0x00 | HDCP_I2C_TO_DIS | HDCP I2C Timeout Disable: Setting this bit to a 1 will disable the bus timeout function in the HDCP I2C master. When enabled, the bus timeout function allows the I2C master to assume the bus is free if no signaling occurs for more than 1 second. | |||
| 5 | Reserved. | ||||||
| 4 | RW | 0x00 | DIS_RI_SYNC | Disable Ri Synchronization check: Ri is normally checked both before and after the start of frame 128. The check at frame 127 ensures synchronization between the two. Setting this bit to a 1 will disable the check at frame 127. | |||
| 3 | RW | RGB_CHKSUM_EN | Enable RBG video line checksum: Enables sending of ones-complement checksum for each 8-bit RBG data channel following end of each video data line. | ||||
| 2 | RW | FC_TESTMODE | Frame Counter Test mode: Speeds up frame counter used for Pj and Ri verification. When set to a 1, Pj is computed every 2 frames and Ri is computed every 16 frames. When set to a 0, Pj is computed every 16 frames and Ri is computed every 128 frames. | ||||
| 1 | RW | TMR_SPEEDUP | Timer Speedup: Speed up HDCP authentication timers. | ||||
| 0 | RW | HDCP_I2C_FAST | HDCP I2C Fast Mode Enable Setting this bit to a 1 will enable the HDCP I2C Master in the HDCP Receiver to operation with Fast mode timing. If set to a 0, the I2C Master will operation with Standard mode timing. This bit is mirrored in the IND_STS register. | ||||
| 194 | 0xC2 | HDCP_CFG | 7 | RW | 0xA8 | ENH_LV | Enable Enhanced Link Verification: Enables enhanced link verification. Allows checking of the encryption Pj value on every 16th frame.
0 = Enhanced Link Verification disabled. 1 = Enhanced Link Verification enabled. |
| 6 | RW | HDCP_EESS | Enable Enhanced Encryption Status Signaling: Enables Enhanced Encryption Status Signaling (EESS) instead of the Original Encryption Status Signaling (OESS).
0 = OESS mode enabled. 1 = EESS mode enabled. |
||||
| 5 | RW | TX_RPTR | Transmit Repeater Enable: Enables the transmitter to act as a repeater. In this mode, the HDCP Transmitter incorporates the additional authentication steps required of an HDCP Repeater.
0 = Transmit Repeater mode disabled. 1 = Transmit Repeater mode enabled. |
||||
| 4:3 | RW | ENC_MODE | Encryption Control Mode: Determines mode for controlling whether encryption is required for video frames.
00 = Enc_Authenticated. 01 = Enc_Reg_Control. 10 = Enc_Always. 11 = Enc_InBand_Control (per frame). |
||||
| 2 | RW | WAIT_100MS | Enable 100MS Wait: The HDCP 1.3 specification allows for a 100Ms wait to allow the HDCP Receiver to compute the initial encryption values. The FPD-Link III implementation guarantees that the Receiver will complete the computations before the HDCP Transmitter. Thus the timer is unnecessary. To enable the 100ms timer, set this bit to a 1. | ||||
| 1 | RW | RX_DET_SEL | RX Detect Select: Controls assertion of the Receiver Detect Interrupt. If set to 0, the Receiver Detect Interrupt will be asserted on detection of an FPD-Link III Receiver. If set to 1, the Receiver Detect Interrupt will also require a receive lock indication from the receiver. | ||||
| 0 | RW | HDCP_AVMUTE | Enable AVMUTE: Setting this bit to a 1 will initiate AVMUTE operation. The transmitter will ignore encryption status controls while in this state. If this bit is set to a 0, normal operation will resume. This bit may only be set if the HDCP_EESS bit is also set. | ||||
| 195 | 0xC3 | HDCP_CTL | 7 | RW | 0x00 | HDCP_RST | HDCP Reset : Setting this bit will reset the HDCP transmitter and dis-able HDCP authentication. This bit is self-clearing. |
| 6 | Reserved. | ||||||
| 5 | RW | 0x00 | KSV_LIST_VALID | KSV List Valid : The controller sets this bit after validating the Repeater’s KSV List against the Key revocation list. This allows completion of the Authentication process. This bit is self-clearing. | |||
| 4 | RW | KSV_VALID | KSV Valid : The controller sets this bit after validating the Receiver’s KSV against the Key revocation list. This allows continuation of the Authentication process. This bit will be cleared upon assertion of the KSV_RDY flag in the HDCP_STS register. Setting this bit to a 0 will have no effect. | ||||
| 3 | RW | HDCP_ENC_DIS | HDCP Encrypt Disable : Disables HDCP encryption. Setting this bit to a 1 will cause video data to be sent without encryption. Authentication status will be maintained. This bit is self-clearing. | ||||
| 2 | RW | HDCP_ENC_EN | HDCP Encrypt Enable : Enables HDCP encryption. When set, if the device is authenticated, encrypted data will be sent. If device is not authenticated, a blue screen will be sent. Encryption should always be enabled when video data requiring content protection is being supplied to the transmitter. When this bit is not set, video data will be sent without encryption. Note that when CFG_ENC_MODE is set to Enc_Always, this bit will be read only with a value of 1. | ||||
| 1 | RW | HDCP_DIS | HDCP Disable: Disables HDCP authentication. Setting this bit to a 1 will disable the HDCP authentication. This bit is self-clearing. | ||||
| 0 | RW | HDCP_EN | HDCP Enable/Restart: Enables HDCP authentication. If HDCP is already enabled, setting this bit to a 1 will restart authentication. Setting this bit to a 0 will have no effect. A register read will return the current HDCP enabled status. | ||||
| 196 | 0xC4 | HDCP_STS | 7 | R | 0x00 | I2C_ERR_DET | HDCP I2C Error Detected: This bit indicates an error was detected on the embedded communications channel with the HDCP Receiver. Setting of this bit might indicate that a problem exists on the link between the HDCP Transmitter and HDCP Receiver. This bit will be cleared on read. |
| 6 | R | RX_INT | RX Interrupt : Status of the RX Interrupt signal. The signal is received from the attached HDCP Receiver and is the status on the INTB_IN pin of the HDCP Receiver. The signal is active low, so a 0 indicates an interrupt condition. | ||||
| 5 | R | RX_LOCK_DET | Receiver Lock Detect : This bit indicates that the downstream Receiver has indicated Receive Lock to incoming serial data. | ||||
| 4 | R | DOWN_HPD | Downstream Hot Plug Detect: This bit indicates a downstream repeater has reported a Hot Plug event, indicating addition of a new receiver. This bit will be cleared on read. | ||||
| 3 | R | RX_DETECT | Receiver Detect : This bit indicates that a downstream Receiver has been detected. | ||||
| 2 | R | KSV_LIST_RDY | HDCP Repeater KSV List Ready : This bit indicates that the Receiver KSV list has been read and is available in the KSV_FIFO registers. The device will wait for the controller to set the KSV_LIST_VALID bit in the HDCP_CTL register before continuing. This bit will be cleared once the controller sets the KSV_LIST_VALID bit. | ||||
| 1 | R | KSV_RDY | HDCP Receiver KSV Ready : This bit indicates that the Receiver KSV has been read and is available in the HDCP_BKSV registers. If the de-vice is not a Repeater, it will wait for the controller to set the KSV_VALID bit in the HDCP_CTL register before continuing. This bit will be cleared once the controller sets the KSV_VALID bit. | ||||
| 0 | R | AUTHED | HDCP Authenticated: Indicates the HDCP authentication has completed successfully. The controller may now send video data requiring content protection. This bit will be cleared if authentication is lost or if the controller restarts authentication. | ||||
| 198 | 0xC6 | ICR | 7 | RW | 0x00 | IE_IND_ACC | Interrupt on Indirect Access Complete: Enables interrupt on completion of Indirect Register Access. |
| 6 | RW | IE_RXDET_INT | Interrupt on Receiver Detect: Enables interrupt on detection of a downstream Receiver. If HDCP_CFG:RX_DET_SEL is set to a 1, the interrupt will wait for Receiver Lock Detect. | ||||
| 5 | RW | IE_RX_INT | Interrupt on Receiver interrupt: Enables interrupt on indication from the HDCP Receiver. Allows propagation of interrupts from downstream devices. | ||||
| 4 | RW | IE_LIST_RDY | Interrupt on KSV List Ready: Enables interrupt on KSV List Ready. | ||||
| 3 | RW | IE_KSV_RDY | Interrupt on KSV Ready: Enables interrupt on KSV Ready. | ||||
| 2 | RW | IE_AUTH_FAIL | Interrupt on Authentication Failure: Enables interrupt on authentication failure or loss of authentication. | ||||
| 1 | RW | IE_AUTH_PASS | Interrupt on Authentication Pass: Enables interrupt on successful completion of authentication. | ||||
| 0 | RW | INT_EN | Global Interrupt Enable: Enables interrupt on the interrupt signal to the controller. | ||||
| 199 | 0xC7 | ISR | 7 | R | 0x00 | IS_IND_ACC | Interrupt on Indirect Access Complete: Indirect Register Access has completed. |
| 6 | R | IS_RXDET_INT | Interrupt on Receiver Detect interrupt: A downstream receiver has been detected. If HDCP_CFG:RX_DET_SEL is set to a 1, the interrupt will wait for Receiver Lock Detect. | ||||
| 5 | R | IS_RX_INT | Interrupt on Receiver interrupt: Receiver has indicated an interrupt request from down-stream device. | ||||
| 4 | R | IS_LIST_RDY | Interrupt on KSV List Ready: The KSV list is ready for reading by the controller. | ||||
| 3 | R | IS_KSV_RDY | Interrupt on KSV Ready: The Receiver KSV is ready for reading by the controller. | ||||
| 2 | R | IS_AUTH_FAIL | Interrupt on Authentication Failure: Authentication failure or loss of authentication has occurred. | ||||
| 1 | R | IS_AUTH_PASS | Interrupt on Authentication Pass: Authentication has completed successfully. | ||||
| 0 | R | INT | Global Interrupt: Set if any enabled interrupt is indicated. | ||||
| 200 | 0xC8 | NVM_CTL | 7 | R | 0x00 | NVM_PASS | NVM Verify pass: This bit indicates the completion status of the NVM verification process. This bit is valid only when NVM_DONE is asserted.
0: NVM Verify failed. 1: NVM Verify passed. |
| 6 | R | NVM_DONE | NVM Verify done: This bit indicates that the NVM Verification has completed. | ||||
| 5 | RW | NVM_PARALLEL | NVM Parallel Load Enable: Setting this bit enables external parallel data to be written to NVM SRAM. Byte data and a memory clock are brought in on the R[7:0] and G[0] pins respectively. In this mode of operation NVM_DATA[0] acts as a memory enable to enable writes to the NVM SRAM. | ||||
| 4:3 | Reserved. | ||||||
| 2 | RW | 0x00 | NVM_VFY | NVM Verify: Setting this bit will enable a verification of the NVM contents. This is done by reading all NVM keys, computing a SHA-1 hash value, and verifying against the SHA-1 hash stored in NVM. This bit will be cleared upon completion of the NVM Verification. | |||
| 1 | RW | NVM_PROG | NVM Program: Setting this bit to a 1 allows programming of the NVM memory from the NVM SRAM. | ||||
| 0 | RW | NVM_PROG_EN | NVM Program Enable: Set to a 1 to allow erase or programming of NVM. | ||||
| 206 | 0xCE | BLUE_SCREEN | 7:0 | RW | 0xFF | BLUE_SCREEN_VAL | Blue Screen Data Value: Provides the 8-bit data value sent on the Blue channel when the HDCP Transmitter is sending a blue screen. |
| 224 | 0xE0 | HDCP_DBG_ALIAS | 7:0 | R | HDCP_DBG | Read-only alias of HDCP_DBG register. | |
| 226 | 0xE2 | HDCP_CFG_ALIAS | 7:0 | R | HDCP_CFG | Read-only alias of HDCP_CFG register. | |
| 227 | 0xE3 | HDCP_CTL_ALIAS | 7:0 | R | HDCP_CTL | Read-only alias of HDCP_CTL register. | |
| 228 | 0xE4 | HDCP_STS_ALIAS | 7:0 | R | HDCP_STS | Read-only alias of HDCP_STS register. | |
| 230 | 0xE6 | HDCP_ICR_ALIAS | 7:0 | R | HDCP_ICR | Read-only alias of HDCP_ICR register. | |
| 231 | 0xE7 | HDCP_ISR_ALIAS | 7:0 | R | HDCP_ISR | Read-only alias of HDCP_ISR register. | |
| 240 | 0xF0 | TX ID | 7:0 | R | 0x5F | ID0 | First byte ID code: "_". |
| 241 | 0xF1 | 7:0 | R | 0x55 | ID1 | Second byte of ID code: "U". | |
| 242 | 0xF2 | 7:0 | R | 0x48 | ID2 | Third byte of ID code: "H". | |
| 243 | 0xF3 | 7:0 | R | 0x39 | ID3 | Fourth byte of ID code: "9". | |
| 244 | 0xF4 | 7:0 | R | 0x32 | ID4 | Fifth byte of ID code: "2". | |
| 245 | 0xF5 | 7:0 | R | 0x39 | ID5 | Sixth byte of ID code: “9”. |
NOTE
Registers 0x40, 0x41, and 0x42 of the Serial Control Bus Registers are used to access the Page 0x10 and 0x14 registers.