The following figures summarize the test results for different sensor packages and PCB configurations, including the following configurations:
- Devices in WCSP BGA package (WCSP)
- Devices in QFN/WSON package with thermal pad
soldered (TPS)
- Devices in QFN/WSON package with no thermal pad
soldered (nTPS)
The following observations come from Figure 5-1:
- Devices in WCSP BGA package (YBG): The
WCSP devices have the highest self-heating offset, which is nearly independent
of board thickness.
- Devices in QFN/WSON package (DRV), with
thermal pad (TP) soldered: The QFN devices with soldered TPs (TPS)
exhibit the lowest self-heating temperatures versus the thermal pad not soldered
(nTPS).
- Board Thickness: The self-heating
temperature is proportional to board thickness, which is expected.
The following observations come from Figure 5-2:
- Devices in WCSP BGA package: The WCSP CBs
have the highest thermal resistance (RT), around 160°C/W. As shown in the TMP117
data sheet, this quantity is attributed to the junction-to-board thermal
resistance of the package. In WCSP parts, most thermal resistance comes from the
WCSP-PCB contacts, and PCB thermal resistance has negligible influence.
- Devices in QFN package, with thermal pad (TP)
soldered: The QFN packaged devices with soldered TPs (TPS) have the
smallest thermal resistance, around 70-80°C/W. According to the TMP117 data
sheet, 35°C/W of this is attributed to the junction-to-board thermal resistance
of the package.
- Effect of PCB Thickness: The thermal
resistance increases as PCB thickness increases, which is expected. This effect
becomes more noticeable when the TP of the QFN package is not soldered.
The following observations come from Figure 5-3:
- Devices in WCSP BGA package: The settling
time for WCSP parts is the smallest, typically 1-3 seconds, despite WCSP parts
having the highest thermal resistance.
- Devices in QFN package, with thermal pad (TP)
soldered: The QFN packaged parts with soldered TPs have the longest
settling time. This is likely due to the increase in thermal mass by the
soldering material now connected to the TPs.
- Effect of Soldering: QFN packaged parts
with soldered TPs on rigid coupon board typically show an increased 30% in
settling time versus non-soldered TP (nTPS).
The following observations can be inferred from
Figure 5-4:
- Devices in 6-mil Flexible PCB: The 6-mil
flexible coupon board exhibits an effective thermal mass close to the package
thermal mass given in the data sheet.
- Devices in QFN package, with thermal pad (TP)
soldered: The QFN packaged parts with TP soldered to 64-mil thickness
coupon board have the highest effective thermal mass, which is 10 times higher
than the WCSP BGA packaged parts assembled on flexible coupon board.
Table 5-1 shows all results across the different tests and calculations are summarized.
Note that the WCSP-6 (YBG) has a package thermal mass of 1mJ/C, and the QFN/WSON
(DRV) package has 5mJ/C:
Table 5-1 Test Results
| Package |
TP Soldered |
PCB |
Effective Thermal Mass (mJ/°C) |
Thermal Resistance (°C/W) |
95% Thermal Response Time (sec) |
15 sec Self-Heat Temp Offset (°C) |
| WCSP-6 /BGA (YBG) |
|
6-mil Flex |
2 |
160 |
1 |
0.9 |
| 32-mil Rigid |
6 |
160 |
2.8 |
0.9 |
| WSON /QFN-6 (DRV) |
Yes |
6-mil Flex |
9 |
62 |
2 |
0.38 |
| 32-mil Rigid |
26 |
82 |
6.8 |
0.59 |
| 64-mil Rigid |
27 |
83 |
7.2 |
0.57 |
| No |
6-mil Flex |
9 |
82 |
2.7 |
0.51 |
| 32-mil Rigid |
14 |
125 |
5.1 |
0.68 |
| 64-mil Rigid |
12 |
148 |
5.1 |
0.87 |