SNOSB21E May   2008  – July 2024 LMH6518

PRODUCTION DATA  

  1.   1
  2. 1 Features
  3. 2 Applications
  4. 3 Description
  5. 4 Pin Configuration and Functions
  6. 5 Specifications
    1. 5.1 Absolute Maximum Ratings
    2. 5.2 ESD Ratings
    3. 5.3 Recommended Operating Conditions
    4. 5.4 Thermal Information
    5. 5.5 Electrical Characteristics
    6. 5.6 Timing Requirements
    7. 5.7 Typical Characteristics
  7. 6 Detailed Description
    1. 6.1 Overview
    2. 6.2 Functional Block Diagram
    3. 6.3 Feature Description
      1. 6.3.1 Input Preamplifier
        1. 6.3.1.1 Primary Output Amplifier
        2. 6.3.1.2 Auxiliary Amplifier
      2. 6.3.2 Overvoltage Clamp
      3. 6.3.3 Attenuator
      4. 6.3.4 Digital Control Block
    4. 6.4 Device Functional Modes
      1. 6.4.1 Primary Amplifier
      2. 6.4.2 Auxiliary Output
    5. 6.5 Programming
      1. 6.5.1 Logic Functions
  8. 7 Application and Implementation
    1. 7.1 Application Information
    2. 7.2 Typical Application
      1. 7.2.1 Oscilloscope Front End
        1. 7.2.1.1 Design Requirements
        2. 7.2.1.2 Detailed Design Procedure
          1. 7.2.1.2.1 Settings and ADC SPI Code (ECM)
          2. 7.2.1.2.2 Input and Output Considerations
            1. 7.2.1.2.2.1 Output Swing, Clamping, and Operation Beyond Full Scale
          3. 7.2.1.2.3 Oscilloscope Trigger Applications
        3. 7.2.1.3 Application Curves
      2. 7.2.2 JFET LNA Implementation
        1. 7.2.2.1 Design Requirements
        2. 7.2.2.2 Detailed Design Procedure
          1. 7.2.2.2.1 Attenuator Design
        3. 7.2.2.3 Application Curve
    3. 7.3 Power Supply Recommendations
    4. 7.4 Layout
      1. 7.4.1 Layout Guidelines
      2. 7.4.2 Layout Example
  9. 8 Device and Documentation Support
    1. 8.1 Device Support
      1. 8.1.1 Third-Party Products Disclaimer
      2. 8.1.2 Device Nomenclature
    2. 8.2 Documentation Support
      1. 8.2.1 Related Documentation
    3. 8.3 Receiving Notification of Documentation Updates
    4. 8.4 Support Resources
    5. 8.5 Trademarks
    6. 8.6 Electrostatic Discharge Caution
    7. 8.7 Glossary
  10. 9 Revision History
  11. 10Mechanical, Packaging, and Orderable Information

Detailed Design Procedure

Figure 7-2 shows a block diagram of the LMH6518 main output signal path.

LMH6518 LMH6518 Signal Path Block DiagramFigure 7-2 LMH6518 Signal Path Block Diagram

The auxiliary output (not shown) uses another but similar output amplifier that taps into the ladder attenuator output. In this data sheet, preamp gain of 30 dB is referred to as high gain (HG), and preamp gain of 10 dB as low gain (LG).

The LMH6518 2-dB/step gain resolution and 40-dB adjustment range (from −1.16 dB to 38.8 dB). These specifications allow this device to be used with the TI GSPS ADCs, which have full scale (FS) adjustment through the extended control mode (ECM) to provide near-continuous variability (8.5-mdB resolution) that covers 42.6-dB FS input range using Equation 1.

Equation 1. LMH6518

TI's GSPS ECM control allows the ADC FS to be set using the ADC SPI bus. The ADC FS voltage range is from 560 mV to 840 mV with 9 bits of FS voltage control.

The ADC ECM gain resolution is calculated with Equation 2.

Equation 2. LMH6518

However, the recommended ADC FS operating range is narrower: from 595 mV to 805 mV with 700 mVPP as the midpoint. Raising the value of ADC FS voltage is tantamount to reducing the signal path gain to accommodate a larger input and vice versa, thus providing a method of gain fine-adjust. The ADC ECM gain adjustment is −1.21-dB, as in Equation 3.

Equation 3. LMH6518

The ADC FS fine-adjust range of 2.62 dB (= 1.41 dB + 1.21 dB) is larger than the LMH6518 2-dB/step resolution; therefore, there is always at least one LMH6518 gain setting to accommodate any FS signal from 6.8 mVPP to 920 mVPP at the LMH6518 input, with 0.62-dB (= 2.62-2) overlap.

Assuming a nominal 0.7-VPP output, the LMH6518 minimum FS input swing is limited by the maximum signal path gain possible and vice versa with Equation 4.

Equation 4. LMH6518

(or 8 mVPP with no ADC fine adjust in Equation 5)

Equation 5. LMH6518

(or 800 mVPP with no ADC FS adjust)

To accommodate a higher FS input, an additional attenuator is required before the LMH6518. This front-end attenuator is shown in the Figure 7-1 with details shown in Figure 7-12. The highest minimum attenuation level is determined by the largest FS input signal (FSmax) in Equation 6.

Equation 6. LMH6518

Therefore, to accommodate 80 VPP, a 40-dB minimum attenuation is required before the LMH6518.

In a typical oscilloscope application, the voltage range encountered is from 1 mV/DIV to 10 V/DIV with eight vertical divisions visible on the screen. One of the primary concerns in a digital oscilloscope is SNR that translates to display trace width to thickness. Typically, oscilloscope manufacturers require the noise level to be low enough so that the no-input visible trace width is less than 1% of FS. Experience shows that this corresponds to a minimum SNR of 52 dB.

The factors that influence SNR are:

  • Scope front-end noise (Front-end attenuator + scope probe Hi-Z buffer which is discussed later in this data sheet and shown in Figure 7-1)
  • LMH6518
  • ADC

The LMH6518 related SNR factors are:

  • Bandwidth
  • Preamp used (Preamp HG or LG)
  • Ladder attenuation
  • Signal level

SNR increases with the inverse square root of the bandwidth. Therefore, reducing bandwidth from 450 MHz to 200 MHz for example, improves SNR by 3.5-dB, as seen in Equation 7.

Equation 7. LMH6518

The other factors listed previously, preamp and ladder attenuation, depend on the signal level and also impact SNR. The combined effect of these factors is summarized in Figure 7-3, where SNR is plotted as a function of the LMH6518 FS input voltage (assuming scope bandwidth of 200-MHz) and not including the ADC and the front-end noise.

LMH6518 LMH6518 SNR and Ladder
                    Attenuation Used vs Input Figure 7-3 LMH6518 SNR and Ladder Attenuation Used vs Input

As Figure 7-3 shows, SNR of at least 52 dB is maintained for FS inputs greater than 24 mVPP (3 mV/DIV on a scope) assuming the LMH6518 internal 200‑MHz filter is enabled. Most oscilloscope manufacturers relax the SNR specifications to 40 dB for the highest gain (lowest scope voltage setting). From Figure 7-3, the LMH6518 minimum SNR is 43.5 dB, thereby meeting the relaxed SNR specification for the lower range of scope front panel voltages.

In Figure 7-3, the step change in SNR near Input FS of 90 mVPP is the transition point from preamp LG to preamp HG with a subsequent 3‑dB difference due to the preamp HG to 20‑dB ladder attenuation lower output noise compared to preamp LG to 2‑dB ladder attenuation noise. Judicious choice of front-end attenuators maintains the 52‑dB SNR specification for scope FS inputs ≥ 24 mVPP by confining the LMH6518 gain range to the lower 30.5‑dB using Equation 8 from the total range of 40‑dB (= 38.8 – (−1.16)) is possible.

Equation 8. LMH6518

For example, to cover the range of 1 mV/DIV to 10 V/DIV (80-dB range), Table 7-1 lists a configuration that affords good SNR.

Table 7-1 Oscilloscope Example Including Front-End Attenuators
ROW SCOPE FS INPUT (VPP) S, SCOPE VERTICAL SCALE (V/DIV) PREAMP LADDER ATTENUATION RANGE (dB) A, FRONT-END ATTENUATION (V/V) MINIMUM SNR (dB) WITH 200 MHz FILTER
1 8 m to 24 m 1 m to 3 m HG 0 to 10 1 44
2 24 m to 80 m 3 m to 10 m HG 10 to 20 1 52
3 80 m to 0.8 10 m to 0.1 LG 0 to 20 1 53.4
4 0.8 to 8 0.1 to 1 LG 0 to 20 10 53.4
5 8 to 80 1 to 10 LG 0 to 20 100 53.4

In Table 7-1, the highest FS input in row 5, column 2 (80 VPP), and the LMH6518 highest FS input allowed (0.8 VPP) set the front-end attenuator value with Equation 9.

Equation 9. LMH6518

The 100 × attenuator allows high-SNR operation down to 30.5‑dB, as explained earlier, or 2.4 VPP at scope input. In that same table, rows 1 to 3 with no front-end attenuation (1 ×) cover the scope FS input range from 8 mVPP to 800 mVPP. That leaves the scope FS input range of 0.8 VPP to 2.4 VPP. If the 100 × attenuator is used for the entire scope FS range of 0.8 VPP to 80 VPP, SNR dips below 52-dB for a portion of that range. Another attenuation level is thus required to maintain the SNR specification requirement of 52 dB.

One possible attenuation partitioning is to select the additional attenuator value to cover a 20 dB range above 0.8 VPP FS (to 8 VPP) with the 100 × attenuator covering the remaining 20‑dB range from 8 VPP to 80 VPP. Mapping 8 VPP FS scope input to 0.8 VPP at LMH6518 input means the additional attenuator is 10 ×, as shown in Table 7-1, row 4. The remaining scope input range of 8 VPP to 80 VPP is then covered by the 100 × front-end attenuator derived earlier. The entire scope input range is now covered with SNR maintained approximately 52 dB for a scope FS input ≥ 24 mVPP, as shown in Table 7-1.