SNOU177 December 2020 LM74700-Q1
When using the LM74700-Q1 as an ORing device, if the input supplies operate at slightly different voltages, the voltage at the common load point will follow the higher voltage. The LM74700-Q1 prevents reverse current flow from the common load point to the lower voltage supply rail. This test uses two LM74700DDFEVMs with 15 V at the input of the first EVM and 12 V at the input of the second EVM and the output of both the EVMs are shorted. As Figure 3-3 shows, the 15-V source at EVM1 is turned off for a period of time and the output (CH2) drops to 12-V source from EVM2. When the 15-V source is turned on again, the output rises to 15 V from EVM1. CH1 shows the input to EVM1, CH2 shows the output and CH3 shows input of EVM2.
Figure 3-3 ORing
Application – Higher Supply SwitchoverNext, the 12-V source at EVM2 is turned off for a period of time and turned on again, the output (CH2) does not change. Figure 3-4 captures this test.
Figure 3-4 ORing
Application 12-V – Lower Supply Test