SNVAAB5 March 2026 LM5190
When the load current is less than the current of Turning point 3, the LM5190 will enter a state of mixed PFM and PWM operation. From the previous content, we know that the logic for turning off the high-side switch in PFM is when the COMP voltage is lower than the clamp value, and the turn-on logic is when the output voltage is lower than a certain threshold. In actual testing, this threshold for the LM5190 is 0.99 times the set output voltage. And the turn-on logic of PWM is the CLK signal high level, and the turn-off logic is when the inductor current reaches the peak.
At this time, the typical working state of LM5190 is shown in Figure 4-1. The load current is 1.407A. It can be clearly seen that there are turn-ons during the output voltage drop process when it is lower than about 12V, such as the turn-on point marked by the white dashed line in the figure. This turn-on logic is typical PFM turn-on, which did not appear before Turning point 3, as shown in Figure 3-2 - Figure 3-5. There are also turn-ons when the output voltage is already in a rising state, which does not meet the PFM turn-on logic. This turn-on logic is typical PWM turn-on, caused by the arrival of the rising edge of CLK.
Figure 4-1 Experimental Results of LM5190 at a Load Current of 1.407AWhen the load current is 0.991A, the phenomenon where PWM and PFM control logic work together is more obvious, as shown in Figure 4-2. Observing its output voltage and inductor current, it can be seen that LM5190 clearly has two turn-on logics at this time. As mentioned before, the one marked by the white dashed line in Figure 4-2 is PFM turn-on, and the one marked by the red dashed line is PWM turn-on.
Figure 4-2 Experimental Results of LM5190 at a Load Current of 0.991A