The PCB layout of any DC-DC converter is critical
to the optimal performance of the design. Bad PCB layout can disrupt the operation
of an otherwise good schematic design. Even if the converter regulates correctly,
bad PCB layout can mean the difference between a robust design and one that cannot
be mass produced. Furthermore, the EMI performance of the converter is dependent on
the PCB layout, to a great extent. In a buck converter, the most critical PCB
feature is the loop formed by the input capacitor or capacitors and power ground, as
shown in Figure 8-62. This loop carries large transient currents that can cause large transient
voltages when reacting with the trace inductance. These unwanted transient voltages
disrupt the proper operation of the converter. Because of this, the traces in this
loop must be wide and short, and the loop area as small as possible to reduce the
parasitic inductance. Figure 8-63 shows a recommended layout for the critical components for the circuit of the
device.
- Place the input capacitor or capacitors as close as possible input pin
pairs: VIN1 to PGND1 and VIN2 to PGND2. Each
pair of pins are adjacent, simplifying the input
capacitor placement. With the VQFN-HR package,
there are two VIN/PGND pairs on either side of the
package, which provides for a symmetrical layout
and helps minimize switching noise and EMI
generation. Use a wide VIN plane on a lower layer
to connect both of the VIN pairs together to the
input supply.
- Place bypass capacitor for VCC close to the VCC pin and AGND pins: This capacitor must routed with short, wide traces to the VCC and AGND pins.
- Use wide traces for the CBOOT capacitor: Place the CBOOT capacitor as
close to the device with short, wide traces to the
CBOOT and SW pins. Route the SW connection under
the device through the gap between VIN2 and RBOOT
pins, reducing exposed SW node area. If an RBOOT
resistor is used, place as close as possible to
CBOOT and RBOOT pins. If high efficiency is
desired, RBOOT and CBOOT pins can be shorted. This
short must be placed as close as possible to RBOOT
and CBOOT pins as possible.
- Place the feedback divider as close as possible to the FB pin of the device: Place RFBB, RFBT, and CFF, if used, physically close to the device. The connections to FB and AGND through RFBB must be short and close to those pins on the device. The connection to VOUT can be somewhat longer. However, this latter trace must not be routed near any noise source (such as the SW node) that can capacitively couple into the feedback path of the converter.
- Layer 2 of the PCB must be a ground plane: This plane acts as a noise shield and a heat dissipation path. Using layer 2 reduces the inclosed area in the input circulating current in the input loop, reducing inductance.
- Provide wide paths for VIN, VOUT, and GND: These paths must be wide and direct as possible to reduce any voltage drops on the input or output paths of the converter and maximizes efficiency.
- Provide enough PCB area for proper heat sinking: Enough copper area must be used to ensure a low RθJA, commensurate with the maximum load current and ambient temperature. Make the top and bottom PCB layers with two-ounce copper and no less than one ounce. If the PCB design uses multiple copper layers (recommended), thermal vias can also be connected to the inner layer heat-spreading ground planes. Note that the package of this device dissipates heat through all pins. Wide traces must be used for all pins except where noise considerations dictate minimization of area.
- Keep switch area small: Keep the copper area connecting the SW pin to the inductor as short and wide as possible. At the same time, the total area of this node must be minimized to help reduce radiated EMI.