SNVU868A September 2023 – April 2024
This section describes how to set up the LP5813-12EVM properly. Items from the following list are required to begin evaluating the LP5813/LP5812:
In the default jumper setting, the board can be evaluated by USB2ANY power directly and does not need an external power supply. Setup connection is demonstrated in Figure 3-1. The setup procedure is as follows:
Figure 2-1 Hardware Connection