SPRADG0 April 2024 AM62P , AM62P-Q1
This section introduces benchmarks for the video codec in AM62P. Specifically, the benchmark focuses on using of the H264 encoder and decoder. The results are collected from a close to real use-case scenario which includes transmitting of a live video stream over UDP using gstreamer pipeline. The setup uses a USB camera with resolution of 1920x1080 and rate of 30FPS. The transmitter side captures the live video stream from the camera, encodes it using codec accelerator with H264 format and transmits the video over UDP. The other side receives the video stream over UDP, decodes and display it on the screen. Both the transmitter and receiver side are executed on the same AM62P device. This shows the codec capability of executing both the encoder and decoder at the same time. The latency of each component in the pipeline can be measured using the gstreamer tracer that outputs live logs of the measurements to a file that you specify.
Following is the gstreamer pipeline for the encoder sider and UDP transmitter side with the gstreamer tracer configured to log the latency measurement at "/run/trace_encode.log".
GST_TRACERS="latency(flags=pipeline+element)" GST_DEBUG=GST_TRACER:7 GST_DEBUG_FILE="/run/trace_encode.log" \
gst-launch-1.0 \
v4l2src device=/dev/video2 ! image/jpeg, width=1920, height=1080, framerate=30/1 ! jpegdec !videoconvert ! v4l2h264enc ! h264parse ! rtph264pay ! udpsink host=$1 port=5000 sync=false
Following is the gstreamer pipeline for the decoder, UDP receiver and display side with the gstreamer tracer configured to log the latency measurement at "/run/trace_decode.log".
GST_TRACERS="latency(flags=element+pipeline)" GST_DEBUG=GST_TRACER:7
GST_DEBUG_FILE=/run/trace_decode.log \
gst-launch-1.0 -v \
udpsrc port=5000 ! 'application/x-rtp, encoding-name=H264, payload=96' !
rtpjitterbuffer latency=50 ! rtph264depay ! h264parse ! v4l2h264dec !
queue ! kmssink driver-name=tidss sync=false plane-id=31
The python script provided at /opt/edgai-gst-apps/seripts/gst_tracers/parse_gst_tracers.py can be used to calculate the average of the latency measurements recorded in the .log files for each component in pipeline. This script can be executed in parallel with the gstreamer pipeline to show live updates of the latency measurements. For instance this is the printout for the decoder side.
root@am62pxx-evm:/opt/edgeai-gst-apps/scripts/gst_tracers/# parse_gst_tracers.py /run/trace_decode.log
.
.
+-----------------------------------------------------------------------------------+
|element latency out-latancy out-fps frames |
+-----------------------------------------------------------------------------------+
|capsfilter0 0.16 27.54 36 30938 |
|rtpjitterbuffer0 0.36 27.53 36 30938 |
|rtph264depay0 0.20 35.86 27 23752 |
|h264parse0 0.26 35.86 27 23752 |
|v4l2h264dec0 48.12 35.86 27 23751 |
|udpsrc0 49.73 35.86 27 23751 |
|queue0 0.75 35.86 27 23751 |
+-----------------------------------------------------------------------------------+
The average latency measurements for the encoder and decoder are shown inVideo Codec Latency.
Codec H264 | Resolution | Latency [ms] |
---|---|---|
Encoder | 1920x1080 | 10.58 |
Decoder | 1920x1080 | 48.12 |