SPRUI97E May 2017 – September 2025
The power requirements of the processor are met by the TPS6590377 Power Management IC (PMIC). The power sequencing requirements of the AM571x processor are also handled by the TPS6590377 PMIC. Figure 2-2 shows the supply connections from the TPS6590377 PMIC to the AM571x processor.
Refer to the AM571x Sitara Processors Silicon Revision 2.0 Data Manual (SPRS957) for more information about the required supply voltages and supply sequencing. Also refer to the TPS659037 Power Management Unit (PMU) for Processor Data Manual (SLIS165) and the TPS659037 User's Guide to Power AM572x and AM571x User’s Guide (SLIU011) for details about its operation.
Note that the production version of the AM571x IDK EVM uses the TPS6590377 PMIC that supplies the voltages needed for the latest silicon version of the AM5718 processor. Beta prototype IDK EVM units used the TPS6590375 PMIC and Alpha prototype IDK EVM units used the TPS6590372 PMIC.