SPRUIG8H January 2018 ā February 2023
Streaming Engines are high speed data connections between the CPU functional units and L2/L3/DDR memory. A streaming engine (SE) is a read-only data connection, which forwards and formats data on the fly. The SE presents data at up-to vector-width-bits per CPU clock in a holding-register. (Current variants of the C7000 have either a 512-bit vector width or a 256-bit vector width.) This holding register can be used like any other global or local register. Since the SE is a read-only engine, the streaming engine register can be used as input to instructions, but an instruction cannot write to the register.
Each SE has one vector-width holding register. Current variants of C7000 have two instances of the SEānamed SE0 and SE1. Thus, there are two streaming engine registers that can be used as an input to instructions.