SPRUIG8J January 2018 – March 2024
The double and
long double data types are stored in a full 64-bit register.
The value is stored in the double-precision floating-point format (binary64) defined
by the IEEE 754 standard. That is, the exponent is 11 bits long, and the mantissa is
52 bits long.