SPRUJ54A june 2023 – july 2023
The F280015x LaunchPad has several power domains that can be connected or isolated from each other with removable shunts. The different 3.3-V and 5-V power domains are described in Figure 3-2 and Figure 3-3.
Table 3-1 describes the usage of the different removable shunts on the LaunchPad board.
| Shunt Identifier | Usage Description |
|---|---|
| JP1, +5V0 | Connects the +5-V power from the USB-C connector (+5V0_USB) to the +5-V power on the XDS110 side of the board (+5V0_XDS110). Bridges the power and ground isolations between the two board sides. |
| JP1, GND | Connects the board Ground on the isolated USB-C connector side of the board (USB_GND) to the rest of the board ground (GND). Bridges the power and ground isolations between the two board sides. |
| JP2, +5V0 | Connects the +5-V power on the XDS110 side of the board (+5V0_XDS110) to the +5-V power on the F2800157 side of the board (+5V0_MCU). |
| JP2, +3V3 | Connects the +3.3-V power on the XDS110 side of the board (+3V3_XDS110) to the +3.3-V power on the F2800157 side of the board (+3V3_MCU). |