SPRUJ86C October 2023 – August 2024
The AM263Px SoC is equipped with two separate Ethernet interfaces. The first interface is a Gigabit Ethernet Switch (CPSW) subsystem that has two ports with selectable MII, RMII, and RGMII interfaces.
Each of the Ethernet interfaces has an associated Management Data Input/Output (MDIO) module for PHY management. The CPSW and PRU-ICSS MDIO signals are to be routed to the PHY based on which port is routed to the PHY. The Control Card includes two analog switches that determine which MDIO module is routed to the on-board PHY or Ethernet add-on board connector.
The Ethernet port from the Gigabit Ethernet Switch (port 2) and Real-Time Ethernet Port that can be configured for PRU0 (PR0_PRU0_MII0) are routed to the same balls on the SoC such that the pinmux configuration determines which peripheral is being used at one time.
The Control Card includes an on-board gigabit Ethernet PHY transceiver (DP83869HMRGZT). For additional details on the on-board PHY, refer to Section 2.11.2.2. There is also an external connector to attach different Ethernet add-on boards for an additional automotive or industrial Ethernet PHY. For additional details about the boards that can be attached to the Ethernet add-on board connector, refer to the respective board user guide.
The Control Card also includes multiple, 1:2 MUX/DEMUX high-speed switches to route all Ethernet ports between the HSEC, on-board Ethernet PHY, and Ethernet add-on board connector. For a complete description of all Ethernet routing for the control card, refer to Section 2.11.2.1.