SPRUJE8D December 2024 – July 2026
Applicable EVM Revisions: E1, A
Issue Description: RGMII booting fails when the DP83867-EVM-AM Industrial PHY Rev A card is used with the AUDIO-AM275-EVM boards.
This issue applies only during the RGMII boot process. During application execution, the software accesses the PHY through MDIO and programmatically configures the correct TX clock skew, thereby avoiding the double skew problem. Additionally, this timing issue is specific to 1000Mbps (Gigabit) link speed operation. At lower link speeds (10Mbps and 100Mbps), the RGMII TX clock timing margins are sufficient to tolerate the cumulative double clock skew, and booting succeeds without any hardware modification.
Root Cause: The DP83867-EVM-AM Industrial PHY Rev A card is configured through hardware strapping to apply a TX clock skew of 2ns on the PHY side. However, the AM62D/AM275 MAC interface already adds TX clock skew by default. This results in a cumulative double clock skew on the RGMII TX clock line, causing timing violations and boot failure.
Workaround: To mitigate this issue, The TX clock skew setting on the PHY card strapping must be changed from 2ns to 0ns, as the MAC side already compensates for the TX clock skew internally. Follow the steps below:
The following figure illustrates the resistor locations on the Industrial PHY card: