SPRUJG0B December 2024 – November 2025 F29H850DM , F29H850TU , F29H859TU-Q1 , F29P329SM-Q1 , F29P589DM-Q1 , F29P589DU-Q1
If FPU64 is available (CPU3 on F29H85x), double-precision floating point operations can be efficiently performed. To enable use of the FPU64, use the compiler option:
-mfpu=f64On the C29, EABI is the only supported executable format. COFF is not supported. With EABI, the double type is 64-bits. User code that contains literal constants (1.54) without a trailing 'f' (1.54f) is interpreted as double precision per the C standard. This leads to implicit conversion of other associated variables to double precision, which negatively impacts performance when FPU64 is not available (CPU3 on F29H85x).
Using the following compiler option generates a warning when the above occurs:
-Wdouble-promotionAlternately, the following compiler option can be used to limit floating-point constants to single-precision. This eliminates the need to add a trailing 'f' to every floating-point constant. However, with this approach, all floating-point constants become single-precision.
-cl-single-precision-constant