SPRUJG0C December 2024 – October 2026 F29H850DM , F29H850TU , F29H859TU-Q1 , F29P329SM-Q1 , F29P589DM-Q1 , F29P589DU-Q1
In signed or unsigned 32-bit or 64-bit integer division, the C '/' operator is implemented by the compiler using the necessary instructions. Three types of division are supported - traditional, Euclidean, and Modulo. Traditional division is natively supported by the C standard and compiler, where the remainder has the sign of the numerator. In modulo (or floored) division, the remainder has the sign of the denominator. Euclidean division is the preferred choice for control operations, where the quotient is linear about 0, and the remainder is always positive.