SPRUJG2A December 2024 – September 2026
The boot mode for the EVM board is defined by two banks of switches SW1 and SW2. This allows for AM62D SoC Boot mode control by either the user (DIP Switch Control).
All the bits of switch (SW1 and SW2) have a weak pull down resistor and a strong pull up resistor as shown in Figure 2-4. Note that OFF setting provides a low logic level (‘0’) and an ON setting provide a high logic level (‘1’).
Figure 2-4 Boot Mode Switch (MMCSD
Boot)The boot mode pins of the SoC have associated alternate functions during normal operation. Hence isolation is provided using Buffer ICs to cater for alternate pin functionality. The output of the buffer is connected to the boot mode pins on the AM62D SoC and the output is enabled only when the boot mode is needed during a reset cycle.
The input to the buffer is connected to the DIP switch circuit and to the output of an I2C I/O Expander set by the test automation circuit. If the test automation circuit controls the boot mode, manually set all the switches to the OFF position. The boot mode buffer is powered by an always ON power supply so that the boot mode remains present even if the SoC is power cycled.
Switch SW1 and SW2 bits [15:0] are used to set the SoC boot mode.
The switch map to the boot mode functions is provided in the following tables.
| Bit15 | Bit14 | Bit13 | Bit12 | Bit11 | Bit10 | Bit9 | Bit8 | Bit7 | Bit6 | Bit5 | Bit4 | Bit3 | Bit2 | Bit1 | Bit0 |
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| Reserved | Reserved | Backup Boot Mode Configuration | Backup Boot Mode | Primary Boot Mode Configuration | Primary Boot Mode | PLL Configuration | |||||||||
| SW2.3 (B2) | SW2.2 (B1) | SW2.1 (B0) | PLL REF CLK (MHz) |
|---|---|---|---|
| OFF | OFF | OFF | 19.2 |
| OFF | OFF | ON | 20 |
| OFF | ON | OFF | 24 |
| OFF | ON | ON | 25 |
| ON | OFF | OFF | 26 |
| ON | OFF | ON | 27 |
| ON | ON | OFF | RSVD |
| ON | ON | ON | RSVD |
| SW2.7 (B6) | SW2.6 (B5) | SW2.5 (B4) | SW2.4 (B3) | Primary Boot Device Selected |
|---|---|---|---|---|
| OFF | OFF | OFF | OFF | Serial NAND |
| OFF | OFF | OFF | ON | OSPI |
| OFF | OFF | ON | OFF | QSPI |
| OFF | OFF | ON | ON | SPI |
| OFF | ON | OFF | OFF | Ethernet RGMII |
| OFF | ON | OFF | ON | Ethernet RMII |
| OFF | ON | ON | OFF | I2C |
| OFF | ON | ON | ON | UART |
| ON | OFF | OFF | OFF | MMC/ SD card |
| ON | OFF | OFF | ON | eMMC |
| ON | OFF | ON | OFF | USB0 |
| ON | OFF | ON | ON | GPMC NAND |
| ON | ON | OFF | OFF | GPMC NOR |
| ON | ON | OFF | ON | Rsvd |
| ON | ON | ON | OFF | xSPI |
| ON | ON | ON | ON | No boot/Dev Boot |
| SW1.2 (B9) | SW1.1 (B8) | SW2.8 (B7) | Primary Boot Mode | |||
|---|---|---|---|---|---|---|
| RVSD |
Read Mode2 |
0: RSVD (Read mode is taken from Read Mode 1) |
Read Mode1 |
0: OSPI/ 1-1-8 Mode (valid only when Read Mode 2 is 0) |
Serial NAND | |
| 1: SPI/ 1-1-1 Mode (Read mode is taken from Read Mode 2 and Read Mode 1 is ignored) |
1: QSPI/ 1-1-4 Mode (valid only when Read Mode 2 is 0) |
|||||
| RVSD | RSVD | Csel | 0: Boot Flash is on CS 0 | OSPI | ||
| 1: Boot Flash is on CS 1 | ||||||
| RVSD | RSVD | Csel | 0: Boot Flash is on CS 0 | QSPI | ||
| 1: Boot Flash is on CS 1 | ||||||
| RVSD | Mode | 0: SPI Mode 0 | Csel | 0: Boot Flash is on CS 0 | SPI | |
| 1: SPI Mode 3 | 1: Boot Flash is on CS 1 | |||||
| 0 | 0 | Link stat | 0: Phy scan used for speed/duplex setup | RGMII1 | ||
| 1: RGMII status register used for speed/ duplex setup | ||||||
| CLKOUT | 0: 50MHz clock not generated on CLKOUT0 | CLK SRC | 0: External clock source | 0 | RMII1 | |
| 1: 50MHz clock generated on CLKOUT0 | 1: Internal clock source | |||||
| Bus reset | 0: Hung bus reset attempt after 1ms | RSVD | Addr | 0: 0x50 | I2C0 | |
| 1: No hung Bus reset attempted | 1: 0x51 | |||||
| RSVD | RSVD | RSVD | UART0 | |||
| 1 | RSVD | Fs/Raw | 0: FileSystem Mode | MMC/SD Card | ||
| 1: Raw Mode | ||||||
| RSVD | RSVD | RSVD | eMMC | |||
| Core Volt | 0: 0.85V Core Voltage | Mode | 0: DFU(Device) | Lane Swap | 0: No swapping of DP/DM | USB |
| 1: 0.75V Core Voltage | 1: MSC(Host) | 1: DP/DM is swapped | ||||
| RSVD | RSVD | RSVD | GPMC NAND | |||
| RSVD | RSVD | RSVD | GPMC NOR | |||
| RSVD | RSVD | RSVD | RSVD | |||
| SFDP | 0: SFDP disabled | Read Cmd | 0: 0x0B Read Command | Mode | 0: 1S-1S-1S mode at 50MHz | xSPI |
| 1: SFDP enabled | 1: 0xEE Read Command | 1:8D-8D-8D mode at 25MHz | ||||
| RSVD |
ARM/ Thumb |
0: ARM mode | No/Dev | 0: Development Boot | No-boot/Dev boot | |
| 1: Thumb mode | 1: No Boot | |||||
| SW1.5 (B12) | SW1.4 (B11) | SW1.3 (B10) | Backup Boot Device Selected |
|---|---|---|---|
| OFF | OFF | OFF | None (No backup mode) |
| OFF | OFF | ON | USB |
| OFF | ON | OFF | Reserved |
| OFF | ON | ON | UART |
| ON | OFF | OFF | Ethernet |
| ON | OFF | ON | MMC/SD |
| ON | ON | OFF | SPI |
| ON | ON | ON | I2C |
| SW1.6 (B13) | Backup Boot Mode | Defaulted Values for Back up Boot Mode | |
|---|---|---|---|
| RSVD | None | ||
| Mode | 0: DFU (Device) | USB |
Core Volt bit = 0 Lane Swap bit = 0 |
| 1: MSC (Host) | |||
| RSVD | RSVD | ||
| RSVD | UART | ||
| Interface | 0: RGMII with internal Delay | Ethernet | Link Stat bit = 0 (If RGMII) |
| 1: RGMII with external clock source | ClkOut bit= 0 and Clksrc bit = 1 (If RMII) | ||
| 1 | MMC | Mode bit = 0 | |
| RSVD | SPI |
Csel bit = 0 Mode = 0 |
|
| RSVD | I2C |
Addr = 0 Bus Rest = 0 |
|