SPRZ570A November   2023  – May 2024 AM263P4 , AM263P4-Q1

 

  1.   1
  2.   Abstract
  3. 1Usage Notes and Advisories Matrices
  4. 2Silicon Revision 1.0 Usage Notes and Advisories
    1. 2.1 Silicon Revision 1.0 Usage Notes
      1.      i2324
    2. 2.2 Silicon Revision 1.0 Advisories
      1.      i2189
      2.      i2310
      3.      i2374
      4.      i2311
      5.      i2345
      6.      i2351
      7.      i2352
      8.      i2353
      9.      i2354
      10.      i2356
      11.      i2357
      12.      i2358
      13.      i2359
      14.      i2383
      15.      i2392
      16.      i2393
      17.      i2394
      18.      i2401
      19.      i2403
      20.      i2404
      21.      i2405
      22.      i2426
      23.      i2427
      24.      i2428
      25.      i2433
      26.      i2438
      27.      i2439
  5. 3Trademarks
  6. 4Revision History

i2403

M4 ROM: SBL redundant boot image feature not supported on HSSE devices

Details:

SBL redundant boot image feature not supported on HSSE devices

Any corruption on the primary image at the following locations , SBL boot fails to boot from redundant flash region

  • Image corruption at middle of the certificate
  • Image corruption at end of the certificate
  • Image corruption at start of the sbl binary
  • Image corruption at middle of the sbl binary
  • Image corruption at End of the sbl binary

Workaround(s):

None.