SPRZ583 May 2026 TMS320F28P551SG
Revisions Affected: 0
If the user is enabling interrupts using the EINT instruction inside an interrupt service routine (ISR) in order to use the nesting feature, then the user must disable the interrupts before exiting the ISR by using the DINT assembly instruction. Failing to do so may cause the bits in the RB register to not be restored correctly, resulting in undefined code behavior.
If the RPTB ASM instruction is not used inside the application, then there is no issue. In the case of C code source, analysis of the generated disassembly would need to be performed to verify this.
If the ISR is coded in C, then the C28x C compiler may take care of the above and no action is required. If the ISR is coded in C28x assembly language, then the above guidance must be followed.
CGT v15.12.2.LTS (released in April 2016) or newer CGT packages addresses this requirement automatically. DINT only needs to be added for earlier revisions of the CGT tools.